KW40Z_Connectivity_Software_1.0.1 (KSDK_1.3.0); IAR 7.50
Some observed potential code issues list:
1. \ConnSw\framework\Bootloader MKW40Z160_cfg.h contains:
* \file MKW40Z160.h
...
/** Kinetis ARM Cortex-M4 model */
#ifndef _MK21D256_CFG_H
#define _MK21D256_CFG_H
...
#endif//MK21D5_CFG_H
expected:
* \file MKW40Z160_cfg.h
....
/** Kinetis ARM Cortex-M0+ model */
#ifndef _MKW40Z160_CFG_H
#define _MKW40Z160_CFG_H
...
#endif//_MKW40Z160_CFG_H
24. ble_general.h defines should be check against standard limits and
should be correlated to values used in gatt_db.h on Peripheral Preferred Connection Parameters Characteristic
/*! Boundary values for the Connection Parameters (Standard GAP) */
#define gcConnectionIntervalMin_c (0x0006)
#define gcConnectionIntervalMax_c (0x0C80)
#define gcConnectionSlaveLatencyMax_c (0x01F3)
#define gcConnectionSupervisionTimeoutMin_c (0x000A)
#define gcConnectionSupervisionTimeoutMax_c (0x0C80)/*! Default values for the Connection Parameters (Preferred) */
/*! connIntervalmin = Conn_Interval_Min * 1.25 ms */
/*! Value of 0xFFFF indicates no specific minimum */
#ifndef gcConnectionIntervalMinDefault_c
#define gcConnectionIntervalMinDefault_c (40)
#endif/*! connIntervalmax = Conn_Interval_Max * 1.25 ms */
/*! Value of 0xFFFF indicates no specific maximum */
#ifndef gcConnectionIntervalMaxDefault_c
#define gcConnectionIntervalMaxDefault_c (160)
#endif#ifndef gcConnectionSlaveLatencyDefault_c
#define gcConnectionSlaveLatencyDefault_c (0)
#endif.........
ble_sig_defines.h
/*! GAP Peripheral Preferred Connection Parameters Characteristic UUID */
/* https://www.bluetooth.com/specifications/gatt/viewer?attributeXmlFile=org.bluetooth.characteristic.g... */
#define gBleSig_GapPpcp_d 0x2A04....
/*! GAP Peripheral Preferred Connection Parameters Characteristic Value Fields */
#define gBleSig_GapPpcp_Bytes_d 8
/* Minimum Connection Interval uint16 6 3200 connInterval_min = Minimum Connection Interval * 1.25 ms */
#define gBleSig_GapPpcp_mci_d 0x0A, 0x00
/* Maximum Connection Interval uint16 6 3200 */
#define gBleSig_GapPpcp_Mci_d 0x10, 0x00
/* Slave Latency uint16 0 1000 */
#define gBleSig_GapPpcp_SL_d 0x64, 0x00
/* Connection Supervision Timeout Multiplier uint16 10 3200 */
#define gBleSig_GapPpcp_cstm_d 0xE2, 0x04
used in gatt_db.h
PRIMARY_SERVICE(service_gap, gBleSig_GenericAccessProfile_d)
....
CHARACTERISTIC(char_ppcp, gBleSig_GapPpcp_d, (gGattCharPropRead_c) )
VALUE(value_ppcp, gBleSig_GapPpcp_d, (gPermissionFlagReadable_c), gBleSig_GapPpcp_Bytes_d ,gBleSig_GapPpcp_mci_d, gBleSig_GapPpcp_Mci_d, gBleSig_GapPpcp_SL_d, gBleSig_GapPpcp_cstm_d)
0x1800 GenericAccessProfile
0x2A04 Peripheral Preferred Connection Parameters Characteristic
25.OtapBootloader.h
\KW40Z_Connectivity_Software_1.0.1\ConnSw\framework\Bootloader\Bootloader_OTAP_Serial\src\OtapSerialBootloader\OtapBootloader.h
the comment, description here is nok
/*
* Name: gFlashProtection_c
* Description: The value for FPROT register. By default the Flash is not Protected
*/
#ifndef gSerialBootloaderEnable_c
#define gSerialBootloaderEnable_c FALSE
#endif
should be
/*
* Name: gSerialBootloaderEnable_c
* Description: Enable UART Serial bootloader. By default FALSE.
*/
26. TimersManager.h
review TMR_StopTimer + TMR_GetRemainingTime behaviour
some defines to add
#define TmrSecondsToMiliseconds( n ) ( ((n) / 1000) )
#define TmrMilisecondsToSeconds( n ) ( ((n) * 1000) )
27. fsl_tsi_driver.h
TSI_DRV_Recalibrate second parameter expected to be uint16_t
Kinetis SDK v.1.3 API Reference Manual
KSDK13APIRM Rev. 0 Sept 2015
page 2655
tsi_status_t TSI_DRV_Recalibrate (uint32_t instance, uint32_t ∗lowestSignal)
Automatically recalibrates all important TSI settings.
page 2664
70.7.7.12 tsi_status_t TSI_DRV_Recalibrate ( uint32_t instance, uint32_t ∗ lowestSignal )
This function forces the driver to start the recalibration procedure for the current operation mode to get the
best possible TSI hardware settings. The computed setting is stored into the operation mode data and can
be loaded and saved by the TSI_DRV_LoadConfiguration or the TSI_DRV_SaveConfiguration functions.
Warning
The function could take more time to return and is blocking.
// Recalibrate current mode
uint16_t signal;
// Recalibrate the mode to get the best performance for this one electrode
if(TSI_DRV_Recalibrate(0, &signal) != kStatus_TSI_Success)
{
// Error, the TSI driver can’t recalibrate this mode
}
platform/drivers/inc/fsl_tsi_driver.h
/*!
* @brief Automatically recalibrates all important TSI settings.
*
* This function forces the driver to start the recalibration procedure
* for the current operation mode to get the best possible TSI hardware settings.
* The computed setting is stored into the operation mode data and can be
* loaded and saved by the @ref TSI_DRV_LoadConfiguration or the @ref TSI_DRV_SaveConfiguration
* functions.
*
* @warning The function could take more time to return
* and is blocking.
*
@code
// Recalibrate current mode
uint16_t signal;
// Recalibrate the mode to get the best performance for this one electrode
if(TSI_DRV_Recalibrate(0, &signal) != kStatus_TSI_Success)
{
// Error, the TSI driver can't recalibrate this mode
}
@endcode
* @param instance The TSI module instance.
* @param lowestSignal The pointer to variable where will be store the lowest signal of all electrodes
* @return An error code or kStatus_TSI_Success.
*/
tsi_status_t TSI_DRV_Recalibrate(uint32_t instance, uint32_t * lowestSignal);
28. framework uses uint32_t instance as first parameter to multiple functions.
As used values for the hw instances don't go after before 3 (like TPM), some are 0 like TSI,...
For speed issue might be 32bits, but to improve memory usage I'll recommend uint8_t.
19. FwkInit.c
#ifndef _FWKINIT_H_
#define _FWKINIT_H_...
#endif /* _FWKINIT_ */
It does not have separate h, but h looks.
#if defined(FWK_SMALL_RAM_CONFIG)
better be changed to
#if (FWK_SMALL_RAM_CONFIG)
so FWK_SMALL_RAM_CONFIG can be set to 0 or 1 (or TRUE/FALSE) easily in app_preinclude.h
* TIMER implementation file for the ARM CORTEX-M4 processor
should be ARM CORTEX-M0+
20. TimersManager.c
why if 0
#if 0
/*
* NAME: PE_LDD_DeviceDataList
* DESCRIPTION: Array of initialized device structures of LDD components.
* VALUES:
*/
LDD_TDeviceData *PE_LDD_DeviceDataList[] = {NULL};
#endif
why multiple #if defined(FWK_SMALL_RAM_CONFIG) and
#if !defined(FWK_SMALL_RAM_CONFIG)
maybe
#if (FWK_SMALL_RAM_CONFIG)
21. app_preinclude.h
should contain all sw switches for
1.KW40Z_Connectivity_Software_1.0.1\ConnSw\framework
2. KW40Z_Connectivity_Software_1.0.1\ConnSw\bluetooth
selected by folder then by file:
Bootloader, Common, DCDC, Flash, FSCI, FunctionLib, GPIOIrq
Keyboard, LED, Lists, LowPower, MemManager, Messaging
ModuleInfo, MWS, NVM, OSAbstraction, OtaSupport, Panic
Reset, RNG, SecLib, SerialManager, Shell, TimersManager, XCVR
for bluetooth
controller, hci_transport, host, profiles, app
/*! *********************************************************************************
* Framework Configuration
********************************************************************************** */
/*! *********************************************************************************
* Common
********************************************************************************** */
/* FwkInit.c */
/* Defines a smaller FWK configuration */
/* Range default not defined */
#define FWK_SMALL_RAM_CONFIG..........
/*! *********************************************************************************
* Bluetooth - BLE Stack Configuration
********************************************************************************** */
/*! *********************************************************************************
* controller
********************************************************************************** */
/*! *********************************************************************************
* hci_transport
********************************************************************************** */
/* hci_transport.h*/
#define APP_SERIAL_INTERFACE_TYPE (gSerialMgrNone_c)
#define APP_SERIAL_INTERFACE_INSTANCE (0)........
22. OtaSupport.c
void OTA_SetNewImageFlag(void)
{
........
if( status != FTFx_OK )
{
return;
}mNewImageReady = FALSE;
}
can be
if( status == FTFx_OK )
{
mNewImageReady = FALSE;
}
same
void OTA_ImageChunkReq(uint32_t offset, uint8_t len, uint16_t devId)
{
.....
if( NULL == pPkt )
{
return;
}
.....
}
and
void OTA_QueryImageReq(uint16_t devId, uint16_t manufacturer, uint16_t imgType, uint32_t fileVersion)
3. TimersManager.h missed osNumberOfTimers count
#define gTmrTotalTimers_c ( gTmrApplicationTimers_c + gTmrStackTimers_c )
should become (?):
gTmrTotalTimers_c ( gTmrApplicationTimers_c + gTmrStackTimers_c + osNumberOfTimers )
4. app_preinclude.h total stack usage, overflow check (?), and how to dimension:
Stack Size values found in project:
#define gTmrTaskStackSize_c 500
#define gSerialTaskStackSize_c 1024
#define gMainThreadStackSize_c 1024
#define gControllerTaskStackSize_c 900
#define gHost_TaskStackSize_c 1300
#define gL2ca_TaskStackSize_c 600
#define gAppIdleTaskStackSize_c (400)
#define gFwkCommonStackSize_c
#define gMacTaskStackSize_c 1280
#define gPhyTaskStackSize_c 600
#define USB_OTG_TASK_STACKSIZE 2000
#define USB_KHCI_TASK_STACKSIZE 3500
#define USB_KHCI_TASK_STACKSIZE 3500
#define USB_KHCI_TASK_STACKSIZE 3500
#define USB_KHCI_TASK_STACKSIZE 3500
5. #ifdef gXcvrXtalTrimEnabled_d to #if (gXcvrXtalTrimEnabled_d) in KW4xXcvrDrv.c and KW3xXcvrDrv.c
#if (gXcvrXtalTrimEnabled_d)
#include "Flash_Adapter.h"
#endif
...
void XcvrInit ( radio_mode_t radioMode )
{
XcvrInit_ModeChg_Common(radioMode,FIRST_INIT);
#if (gXcvrXtalTrimEnabled_d)
if( 0xFFFFFFFF != gHardwareParameters.xtalTrim )
{
XcvrSetXtalTrim( (uint8_t)gHardwareParameters.xtalTrim );
}
#endif
6. file Eeprom_Boot.h contains:
* \file Eeprom.h
...
#ifndef _EEPROM_H_
#define _EEPROM_H_
...
#endif /* _EEPROM_H_ */
expected
* \file Eeprom_Boot.h
...
#ifndef _EEPROM_BOOT_H_
#define _EEPROM_BOOT_H_
...
#endif /* _EEPROM_BOOT_H_ */
8. ble_sig_defines.h should include DESCRIPTOR support for gatt_db.h
https://www.bluetooth.com/specifications/gatt/descriptors
https://www.bluetooth.com/specifications/gatt/viewer?attributeXmlFile=org.bluetooth.descriptor.gatt....
example:
CHARACTERISTIC(char_temperature, gBleSig_Temperature_d, (gGattCharPropRead_c | gGattCharPropNotify_c))
VALUE(value_temperature, gBleSig_Temperature_d, (gPermissionFlagReadable_c), 2, 0x00, 0xB4)
DESCRIPTOR(desc_temperature, gBleSig_CharPresFormatDescriptor_d, (gPermissionFlagReadable_c), gBleSig_CharPresFormatDescriptorBytes_d, gBleSig_signed_16_bit_integer_d, gBleSig_Exponent_neg2_d, gBleSig_Celsius_temperature_d, gBleSig_No_Namespaces_d, gBleSig_unknown_d)
CCCD(cccd_core_temperature)
based on:
/* DESCRIPTOR(.., gBleSig_CharPresFormatDescriptor_d, .., 7, Format, Exponent, Unit, Namespace, Description)
* https://www.bluetooth.com/specifications/gatt/viewer?attributeXmlFile=org.bluetooth.descriptor.gatt....
* The actual value = Characteristic Value * 10^Exponent. */
#define gBleSig_CharPresFormatDescriptorBytes_d 7
/* Format Mandatory 8bit range 0x00 0x1B */
/* https://www.bluetooth.com/specifications/assigned-numbers/format-types */
/* 4 unsigned 8-bit integer */
#define gBleSig_unsigned_8_bit_integer 0x04
/* 14 signed 16-bit integer */
#define gBleSig_signed_16_bit_integer_d 0x0E
/* Exponent Mandatory sint8 -128 0 127 */
/* 10^Exponent: 0 =1 */
#define gBleSig_Exponent_0_d 0x00
/* 10^Exponent: -2 */
#define gBleSig_Exponent_neg2_d 0xFE
/* 10^Exponent: -3 */
#define gBleSig_Exponent_neg3_d 0xFD
/* Unit The Unit is a UUID. Mandatory uint16 N/A N/A */
/* https://www.bluetooth.com/specifications/assigned-numbers/units */
/* 0x2700 unitless org.bluetooth.unit.unitless */
#define gBleSig_unitless_d 0x00, 0x27
/* 0x272F Celsius temperature (degree Celsius) org.bluetooth.unit.thermodynamic_temperature.degree_celsius */
#define gBleSig_Celsius_temperature_d 0x2F, 0x27
/* 0x2728 electric potential difference (volt) org.bluetooth.unit.electric_potential_difference.volt */
#define gBleSig_electric_potential_difference_d 0x28, 0x27
/* Namespace (organization) Mandatory 8bit 0 1 */
/* 0 No Namespace */
#define gBleSig_No_Namespaces_d 0x00
/* 1 Bluetooth SIG Assigned Numbers */
#define gBleSig_Bluetooth_SIG_Assigned_Numbers_d 0x01
/* Description Name Space field. Mandatory 16bit N/A N/A */
/* https://www.bluetooth.com/specifications/assigned-numbers/gatt-namespace-descriptors */
/* unknown 0x0000 */
#define gBleSig_unknown_d 0x00, 0x00
9. LED inverse output setting (LED1..LED4)
LED.h
/*
* Name: mLEDInvertedOut
* Description: Led outpus inverted. Default value TRUE.
* TRUE
* LedOn -> GPIO_DRV_ClearPinOutput(kGpioLEDx)
* LedOff -> GPIO_DRV_SetPinOutput(kGpioLEDx)
* FALSE
* LedOn -> GPIO_DRV_SetPinOutput(kGpioLEDx)
* LedOff -> GPIO_DRV_ClearPinOutput(kGpioLEDx)
*/
#ifndef mLEDInvertedOut_c
#define mLEDInvertedOut_c TRUE
#endif
LED.c
void LED_Operate
...
case gLedOn_c:
#if (mLEDInvertedOut_c)
GPIO_DRV_ClearPinOutput(kGpioLED1);
#else
GPIO_DRV_SetPinOutput(kGpioLED1);
#endif /* mLEDInvertedOut_c */
break;
case gLedOff_c:
#if (mLEDInvertedOut_c)
GPIO_DRV_SetPinOutput(kGpioLED1);
#else
GPIO_DRV_ClearPinOutput(kGpioLED1);
#endif /* mLEDInvertedOut_c */
break;
....
* \file LED.h
* LED export interface file for ARM CORTEX-M4 processor
should be updated to ARM Cortex-M0+
10. missing _FWKINIT_H_ in FwkInit.c
should add:
...
#ifndef _FWKINIT_H_
#define _FWKINIT_H_
...
#endif /* _FWKINIT_ */
and
* TIMER implementation file for the ARM CORTEX-M4 processor
should be:
* TIMER implementation file for the ARM CORTEX-M0+ processor