I'm trying to use the I2C_DRV_MasterXXXDataBlocking parameters and need some clarification. The following is my interpretation and I would like comments for clarification. (My environment is Windows7, KDS, KSDK, PE, and MQX on FRDM-K22F.)
The documentation states (simplified with my annotation):
====
I2C_DRV_MasterReceiveDataBlocking (
instance, // Which I2C Bus
device, // Address on I2C bus (7-bit width)
cmdBuff, // If not NULL, commands to be sent
cmdSize, // If not zero, number of bytes sent as command IF cmdBuff is not NULL
// If command was sent, a restart applied
// and I2C Address sent with a READ cycle
rxBuff, // Memory location for data read
rxSize, // Number of bytes to read , unless terminated by device
timeout_ms );// Time out in milliseconds (API states microseconds!)
====
My question is: If cmdBuff is NULL, does the driver issue a read to the device without sending out the command first? In other words, the restart cycle is never performed.
I have the same question on the I2C_DRV_MasterReadDataBlocking() function as well.
In these cases I would expect to see the I2C bus go immediately into the appropriate transfer. Am I correct in this interpretation?
Thanks
解決済! 解決策の投稿を見る。
Hi David,
In the case you mention (passing NULL for cmdBuff and cmdSize), you should NOT see a repeated start. The device would expect to start receiving data from the slave immediately.
Regards,
Chris
Hi David,
In the case you mention (passing NULL for cmdBuff and cmdSize), you should NOT see a repeated start. The device would expect to start receiving data from the slave immediately.
Regards,
Chris