BLDC control project based on AN4862

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BLDC control project based on AN4862

680 Views
fazhichen
Contributor I

Hello,

I'm now doing a BLDC control project based on AN4862 . I have modified the EVB for my appliction, so i have some questions about softrware.

i want to define the current AMP gain by myself , how can i modify the code, in which source code file can i find the definition ? Is there a function or formula to calculate actual current .

i want to define the divider resistor of BEMF by myself , how can i modify the code, in which source code file can i find the definition ?

The motor can running , but the sound and the temperature are not normall (SlowControlloop) , what parameters can lead this ?

Looking forward to haear from you .

thanks !

Labels (1)
0 Kudos
1 Reply

433 Views
mohammad_kamil
NXP Employee
NXP Employee

Hello Fazhi Chen,
Please refer DRM144, and AN4870. I hope that will answer all your question. 

0 Kudos