i am using ke06z128vlk4 mcu,and i would like to know, which pin is DAC output pin in mcu.
Refer the attachment(screenshot.png), as in the attachment ==> PTA0 pin is for ACMP0_IN0
then which pin will be for DAC output.
I have also attached the reference manual of ke06.
Thank you
解決済! 解決策の投稿を見る。
Hi
Sorry. There is not DAC output pin.
The 6-bit DAC is 64-tap resistor ladder network which provides a selectable voltage reference for applications where voltage reference is needed.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hii Robin_shen,
Thank you for the answer.
Hi
Sorry. There is not DAC output pin.
The 6-bit DAC is 64-tap resistor ladder network which provides a selectable voltage reference for applications where voltage reference is needed.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------