ov5640 mipi camera not detected on imx8mqevk board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ov5640 mipi camera not detected on imx8mqevk board

441 Views
dngnstjd
Contributor II

Hi, I'm working gstreamer using imx8mqevk.

My goal is rtp streaming.

But, I have a camera not detected problem.

Please refer to below the capture.

pastedImage_5.png

I confirmed that the camera works well in kernel version 4.9.88 and yocto version is imx-linux-rocko.

To achieve my goal, I upgrade yocto version and add PACKAGECONFIG_mx8mq = "x264" in local.conf.

(Because imx8m don`t have H/W encoder. I want use S/W encoder.)

My kernel version is 4.14.98 and yocto version is imx-linux-sumo(manifest is "imx-4.14.98-2.0.0_ga.xml")

Yours solution is my pleasure!!!!!

Thank you!!!

0 Kudos
1 Reply

368 Views
joanxie
NXP TechSupport
NXP TechSupport

what dts file do you use?did you use the dts file with camera?

0 Kudos