low power industrial grade controller with two 10/100 FE Ethernet MAC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

low power industrial grade controller with two 10/100 FE Ethernet MAC

554件の閲覧回数
arunkuna
Contributor I

Hi, I need low power industrial grade( operating temp -40 to 105C) controller with two 10/100 FE Ethernet MAC. Kindly suggest appropriate parts.

0 件の賞賛
4 返答(返信)

398件の閲覧回数
mjbcswitzerland
Specialist V

Hi

If you need to use Kinetis there are a couple of possibilities:

- add extra SPI (or parallel) connected Ethernet controllers - eg. https://community.nxp.com/message/504096
- use a Micrel KSZ8863 PHY and use its tail-tagging mode to create two independent Ethernet interfaces from a single Ethernet controller in a Kinetis part https://community.nxp.com/message/445668?commentID=445668#comment-445668

Both of these modes, and multi-homed networking, are fully integrated into the uTasker Kinetis project in case you also need a proven and immediately operational software solution to go with the hardware.... (also with integrated low power support of Kinetis part during operation).

Regards

Mark
Kinetis for professionals: http://www.utasker.com/kinetis.html

0 件の賞賛

398件の閲覧回数
cutworth
NXP Employee
NXP Employee

Hi Arun,

You can check the following page for dual Ethernet MAC support.

MCF5441X|32 Bit Microcontroller (MCU)|NXP or VF5xx MPUs with ARM Cortex-A5 Core|Vybrid|NXP 

Or if you insist using Kinetis, you can choose ARM Cortex-M4|Kinetis K64 120 MHz 32-bit MCUs|NXP and use Flexbus module to connect DM9000 for adding one more Ethernet interface.

Hao

0 件の賞賛

398件の閲覧回数
lucianomoretti
Contributor IV

As Fang said, there are no Kinetis parts with 2 Ethernet ports. Do you really need 2 separate networks, or could you put an ethernet switch chip on your board to give you the ports you need?

0 件の賞賛

398件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

Sorry,  for Kinetis and LPC family, there has no parts with 2 Ethernet MAC. And we have I.MX parts has two ethernets, but it is not low power nor industrial grade( operating temp -40 to 105C). Sorry.

0 件の賞賛