Hi all,
i am trying to debug my app via osbdm on twr-k60n512.
i am using openocd(version 0.6.0), and the target is recognized well.
also some basic commands like "reset init" or "target halt" works fine(in terminal).
Info : OSBDM has opened
Info : clock speed 1 kHz
Info : JTAG tap: k60.cpu tap/device found: 0x4ba00477 (mfg: 0x23b, part: 0xba00, ver: 0x4)
Info : k60.cpu: hardware has 6 breakpoints, 4 watchpoints
when i am starting debugger in eclipse it's look OK but when i press RESUME i've got
target halted due to debug-request, current mode: Thread
xPSR: 0x01000000 pc: 0xfffffffe msp: 0xfffffffc
Error: GDB missing ack(2) - assumed good
Warn : acknowledgment received, but no packet pending
Warn : keep_alive() was not invoked in the 1000ms timelimit. GDB alive packet not sent! (1001). Workaround: increase "set remotetimeout" in GDB
i am using arm-eabi-gdb debugger with this commands:
target remote localhost:3333
monitor reset init
monitor halt
load
break main
am i missing something?
best regards,
Filip.