is kinetis k40 internal voltage regulator internally connected to core?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

is kinetis k40 internal voltage regulator internally connected to core?

733 次查看
pablo_slavkin
Contributor I

Hi, I'm trying to use the internal voltage regulator of the k40, but I don't know if  I'd wire on on the PCB the 3v3out to all VDD of the IC to get the uC run.... or if it's internally connected to the core and peripherals. and let the VDD pins unconnected..

I could't find the block diagram of the internall setup so I'm confusing....

thanks in advance for your time.

Pablo

0 项奖励
回复
2 回复数

603 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Pablo:

I think you refer to USB regulator, right?

This regulator is not internally connected to the core or peripherals, so yes, you need to wire externally to VDD. Just place a capacitor between Vreg33out and GND (~ 2.2 uF). AND make sure not to exceed the maximum 120 mA.


Regards!
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

603 次查看
Wlodek_D_
Senior Contributor II

Hello,

Thank you for your post, however please consider moving it to the right community place (e.g. Kinetis Microcontrollers ) to get it visible for active members.

For details please see general advice Where to post a Discussion?

Thank you for using Freescale Community.

0 项奖励
回复