expansion boards for a kinetis 64 board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

expansion boards for a kinetis 64 board

1,245 次查看
randyseedle
Contributor III

Are there any expansion boards out there that use the kinetis specific I/O pins ?

标签 (1)
0 项奖励
3 回复数

965 次查看
randyseedle
Contributor III

Hmmm, so is a good document describing the inner row of pins ?

0 项奖励

965 次查看
BlackNight
NXP Employee
NXP Employee

AFIK there is no dedicated document for this, and now standard. Every board has different pins on the inner rows. The best document for it is is the schematics PDF.

965 次查看
BlackNight
NXP Employee
NXP Employee

Hello,

not sure what you mean with Kinetis specific I/O pins? Or do you mean the inner rows? They make sense if you develop your own board. I'm not aware of any commercial boards which use them. The outer 'standard' rows can be used with all the 'Arduino' shields as long they are designed to work with 3.3V logic levels.

I hope this helps,

Erich

0 项奖励