expansion boards for a kinetis 64 board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

expansion boards for a kinetis 64 board

1,230 Views
randyseedle
Contributor III

Are there any expansion boards out there that use the kinetis specific I/O pins ?

Labels (1)
0 Kudos
3 Replies

950 Views
randyseedle
Contributor III

Hmmm, so is a good document describing the inner row of pins ?

0 Kudos

950 Views
BlackNight
NXP Employee
NXP Employee

AFIK there is no dedicated document for this, and now standard. Every board has different pins on the inner rows. The best document for it is is the schematics PDF.

950 Views
BlackNight
NXP Employee
NXP Employee

Hello,

not sure what you mean with Kinetis specific I/O pins? Or do you mean the inner rows? They make sense if you develop your own board. I'm not aware of any commercial boards which use them. The outer 'standard' rows can be used with all the 'Arduino' shields as long they are designed to work with 3.3V logic levels.

I hope this helps,

Erich

0 Kudos