Will OpenThread bring KDS support to KW family?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Will OpenThread bring KDS support to KW family?

551 Views
JonathanHess
Contributor III

Note the references to NXP in the Nest OpenThread press release:

Nest Announces Open Source Implementation of Thread | Nest

I've not tried to compile but the source has #if's for __GNUC__ which means gcc which hopefully means the ARM supplied gcc in KDS.

I also spied references to "class", and a few "virtual"s which makes me hope OpenThread would be friendly to C++.

My quick perusal could not identify or locate any hardware/soc specific code so I don't know if the claim of NXP (presumably KW) support was more "could happen" or "works out of the box."

Anyone else know?

The idea of real KW support via KDS rather than IAR has appeal to me.  As does avoiding BeeKit and its codegen wizards.

Labels (1)
0 Kudos
1 Reply

327 Views
miduo
NXP Employee
NXP Employee

Hi,

At present, there has no any plan to support the KW family with KDS, only the IAR is applicable. Anyway, as you deeped dive, there has an interesting post maybe you would like to have a look:

https://community.nxp.com/message/611022#comment-611022

0 Kudos