Hello, I am using TWR-KV58F220M with TWR-MC-LV3PH board and motor control package MCRSP_PMSM_V1.2.0. I am checking out the ADC connections for the motor control. I have found the following measurement channels:
M1_ADC0_PH_A (2)
M1_ADC1_PH_A (2)
M1_ADC1_PH_B (3)
M1_ADC0_PH_C (7)
M1_ADC0_UDCB (6)
M1_ADC1_AUX (6)
I am wondering what is the AUX signal, because I haven't found any explanation about it.
It would be great, if anyone can help me with this question.
BR, Risto
Hi Risto,
Please refer below information descripted in AN5237.
Best Regards,
Robin
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------