What are the preferred connections for unused pins one K20DX256V?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What are the preferred connections for unused pins one K20DX256V?

459件の閲覧回数
elizabethamyoun
Contributor I

What are the preferred connections for unused pins one K20DX256V?

ラベル(1)
0 件の賞賛
返信
1 返信

287件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello Elizabeth,

For the Kinetis family it is recommended to leave unused pines floating and configure them as disabled.

In the below document you can find some tips and tricks to consider when designing for low power.

https://developer.mbed.org/media/uploads/GregC/an4470-using_low-power_modes_with_kinetis_mcus.pdf

I hope this helps,


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信