What are the preferred connections for unused pins one K20DX256V?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What are the preferred connections for unused pins one K20DX256V?

544 次查看
elizabethamyoun
Contributor I

What are the preferred connections for unused pins one K20DX256V?

标签 (1)
0 项奖励
回复
1 回复

372 次查看
soledad
NXP Employee
NXP Employee

Hello Elizabeth,

For the Kinetis family it is recommended to leave unused pines floating and configure them as disabled.

In the below document you can find some tips and tricks to consider when designing for low power.

https://developer.mbed.org/media/uploads/GregC/an4470-using_low-power_modes_with_kinetis_mcus.pdf

I hope this helps,


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复