Trying to get a KL27 Freescale processor to wake up from a low power (LLS) state on a I/O pin's falling edge. However, as best as I can tell, the processor current demand returns, but the processor does not continue to execute the program.
If I leave the debugger connected (which draws about 80uA of additional current) I can run the program into LLS mode, then press a switch which drops the voltage on I/O pin C1. The processor current demand returns to several mAs. But the LED flashing behavior indicating the processor has continued executing code never occurs. If I break the program using the debugger, I see it has stopped on the line of code following the WFI (Wait For Interrupt) line of code. (I can repeat this test with the same results with the debugger not operating. Of course I then have no way to know for sure where the program is hung.)
I was expecting the interrupt service routine for the LLWU (Low Leakage Wake Up) feature to execute. This should have flashed the blue LED. Then for the execution of the code to continue in the main() routine flashing the red LED. Then for the KL27 processor to return to low power mode waiting for the next button press which would have dropped the voltage on I/O pin C1. Instead the (as stated above) the processor current demand returns and subsequent button presses changes nothing. No LED activity and no current changes.
So additional code to detect activity on ports B, C, D or E was added. The service routine for this feature flashes a green LED. Now the behavior is very different. Upon the first button press the current raises from 2.3uA to 1.9mA. But there is no LED activity. Upon the second button press the green LED flashes then the red LED flashes then the current drops to 2.3uA. Guessing, the processor exits the LLS state after the first button press but does not execute any code. Then, the second button press causes the PORTBCDE_IRQHandler to be called. This flashes the green LED. Then execution continues in the main routine flashing the red LED. And finally the processor returns to LLS mode.
Why?
Why does the processor demand much more current but apparently not execute any code after first I/O pin C1 transitions from high to low?
(All tests and code were executed on a Freescale FRDM-KL27Z development board.)
-thanks
Code:
// start of code
// INCLUDES /////////////////////////////////////////////////////////
//-------------------------------------------------------------------
#include "MKL27Z644.h" // KL27 M0+ register definitions
// FUNCTION HEADERS /////////////////////////////////////////////////
//-------------------------------------------------------------------
void MCU_Init(void); // initializes MCU for Freedom Board
void MCU_Delay(uint32_t delay); // delay in multiples of 1ms
//---------------------------------------------------------------------
void RGB(uint8_t Red,uint8_t Green,uint8_t Blue); // RGB-LED Control: 1=on, 0=off, for each of the 3 colors
// *** MAIN *********************************************************
//-------------------------------------------------------------------
int main(void)
{
MCU_Init(); // MCU Initialization; has to be done prior to anything else
RGB(0,0,0); // Start with all LEDs off
__asm("CPSIE i"); // Enable all Interrupts
NVIC->ICPR[0] = (uint32_t)(1 << (PORTBCDE_IRQn & 0x1F)); // Clear PORTBCDE Interrupt in NVIC Core register
NVIC->ISER[0] = (uint32_t)(1 << (PORTBCDE_IRQn & 0x1F)); // Set PORTBCDE Interrupt in NVIC Core register
volatile int dummyread;
RGB(0,0,0);
SMC_PMPROT = SMC_PMPROT_ALLS_MASK;
SMC_PMCTRL = SMC_PMCTRL_STOPM(3); // (MC2) Set STOPM = 0b11
// Enable hi to lo transition for LLWU_P6 / pin-C1.
LLWU_PE2 = 0x20;
// Set the SLEEPDEEP bit to enable deep sleep mode.
// (W/o this we only drop to about 3.1mA down from 4.6mA.)
SCB->SCR |= SCB_SCR_SLEEPDEEP_Msk;
for(;;)
{
// Clear WUF6 (aka LLWU_P6) by writing a 1 to the flag bit.
// (Need to do this to get the uC down from drawing ~2-3mA to <5uA.
LLWU_F1 = 0x40;
RGB(0,0,0);
__asm("WFI"); // Enter low power mode
dummyread = PMC_REGSC;
GPIOB_PTOR|=(1<<18); // Toggle RED LED
MCU_Delay(200);
}
}
//-------------------------------------------------------------------
// ******************************************************************
// FUNCTION BODIES //////////////////////////////////////////////////
//-------------------------------------------------------------------
void MCU_Init(void)
{
// Crucial
__asm("CPSID i"); // Disable interrupts
//Disable Watchdog
SIM_COPC=0x00; // Disable COP watchdog
//System Registers
SIM_SCGC5|=SIM_SCGC5_PORTA_MASK; // Enable PortA clock
SIM_SCGC5|=SIM_SCGC5_PORTB_MASK; // Enable PortB clock
SIM_SCGC5|=SIM_SCGC5_PORTC_MASK; // Enable PortC clock
SIM_SCGC5|=SIM_SCGC5_PORTD_MASK; // Enable PortD clock
SIM_SCGC5|=SIM_SCGC5_PORTE_MASK; // Enable PortE clock
// System clock initialization
MCG_MC|=MCG_MC_HIRCEN_MASK; // Enable 48MHz HIRC
MCG_C1=MCG_C1_CLKS(0); // Enable Main Clock Source of the 48MHz HIRC
SIM_CLKDIV1&=~(SIM_CLKDIV1_OUTDIV1(1)); // Set Core Clock/1=48MHz
SIM_CLKDIV1|=(SIM_CLKDIV1_OUTDIV4(1)); // Set Bus Clock/2=24MHz
// System Tick Init
SysTick->CTRL=0; // Disable the SysTick Timer
SysTick->LOAD=48000; // Core Clock/1=48MHz, Period=1ms/(1/48000000Hz)=48000
SysTick->VAL=0; // Clear the current counter value to 0
SysTick->CTRL=(SysTick_CTRL_ENABLE_Msk
|SysTick_CTRL_CLKSOURCE_Msk); // Enable SYS TICK timer and set clock source to processor clock (core clock)
// GPIO Init
PORTC->PCR[1] |= PORT_PCR_MUX(1)| // Enable Port Pin PTC1 as GPIO
PORT_PCR_PE_MASK| // Select the resistor to pull up or down on port pin
PORT_PCR_PS_MASK| // Select a pull up resistor
PORT_PCR_IRQC(0x08); // Configure interrupt pin to trigger on a logic low (0)
GPIOC->PDDR&=~(1<<1); // make sure GPIO PTC1 pin is configured as an input
PORTB_PCR18=PORT_PCR_MUX(1); // Set Pin B18 to GPIO function
PORTB_PCR19=PORT_PCR_MUX(1); // Set Pin B19 to GPIO function
PORTA_PCR13=PORT_PCR_MUX(1); // Set Pin A13 to GPIO function
GPIOB_PDDR|=(1<<18); // Set Pin B18 as output
GPIOB_PDDR|=(1<<19); // Set Pin B19 as output
GPIOA_PDDR|=(1<<13); // Set Pin A13 as output
}
//---------------------------------------------------------------------
void MCU_Delay (uint32_t delay) // Delay in multiples of 1ms (e.g. use 1000 for 1 second)
{
uint32_t delw;
for (delw=0;delw<delay;delw++)
{
while (!(SysTick->CTRL&SysTick_CTRL_COUNTFLAG_Msk));
}
}
//---------------------------------------------------------------------
void RGB(uint8_t Red,uint8_t Green,uint8_t Blue) // RGB-LED Control: 1=on, 0=off, for each of the 3 colors
{
if (Red ==1) GPIOB_PCOR|=(1<<18); else GPIOB_PSOR|=(1<<18);
if (Green ==1) GPIOB_PCOR|=(1<<19); else GPIOB_PSOR|=(1<<19);
if (Blue ==1) GPIOA_PCOR|=(1<<13); else GPIOA_PSOR|=(1<<13);
}
//---------------------------------------------------------------------
// INTERRUPT BODIES /////////////////////////////////////////////////
//-------------------------------------------------------------------
void PORTBCDE_IRQHandler (void)
{
PORTC->PCR[1]|= PORT_PCR_ISF_MASK; // Clear interrupt flag
GPIOB_PTOR|=(1<<19); // Toggle GREEN LED
MCU_Delay(200); // Delay 200ms
}
void LLWU_IRQHandler (void)
{
GPIOB_PTOR|=(1<<13); // Toggle BLUE LED
MCU_Delay(200); // Delay 200ms
}
// end of code
解決済! 解決策の投稿を見る。
Hi Rick
In your LLWU interrupt handler check the source of the wake up (in your case it will only be the single LLWU_Px that you programmed) and reset its interrupt flag by writing a '1' back to it (i.e put LLWU_F1 = 0x40; into LLWU_IRQHandler() as well).
This will probably solve your difficulty because if you don't reset the interrupt flag you will find that the processor is jumping in and out of this interrupt routine forever (and look to be hanging) rather than continuing with the code flow.
Get developer's information to the LLWU at http://www.utasker.com/kinetis/LLWU.html
Regards
Mark
Kinetis: µTasker Kinetis support
KL25: µTasker Kinetis FRDM-KL25Z support / µTasker Kinetis TWR-KL25Z48M support
KL26: µTasker Kinetis FRDM-KL26Z support / µTasker Kinetis Teensy LC support
For the complete "out-of-the-box" Kinetis experience and faster time to market
Hi Rick
In your LLWU interrupt handler check the source of the wake up (in your case it will only be the single LLWU_Px that you programmed) and reset its interrupt flag by writing a '1' back to it (i.e put LLWU_F1 = 0x40; into LLWU_IRQHandler() as well).
This will probably solve your difficulty because if you don't reset the interrupt flag you will find that the processor is jumping in and out of this interrupt routine forever (and look to be hanging) rather than continuing with the code flow.
Get developer's information to the LLWU at http://www.utasker.com/kinetis/LLWU.html
Regards
Mark
Kinetis: µTasker Kinetis support
KL25: µTasker Kinetis FRDM-KL25Z support / µTasker Kinetis TWR-KL25Z48M support
KL26: µTasker Kinetis FRDM-KL26Z support / µTasker Kinetis Teensy LC support
For the complete "out-of-the-box" Kinetis experience and faster time to market
Thanks Mark, I cleaned up the code. Also missing was code to enable LLWU interrupts. To close out this thread here is the working code (using SW3 on a FRDM-KL27Z Freescale board to wake up the processor from LLS mode and flash the RGB LED to indicate activity):
// code start
// INCLUDES /////////////////////////////////////////////////////////
//-------------------------------------------------------------------
#include "MKL27Z644.h" // KL27 M0+ register definitions
// FUNCTION HEADERS /////////////////////////////////////////////////
//-------------------------------------------------------------------
void MCU_Init(void); // initializes MCU for Freedom Board
void MCU_Delay(uint32_t delay); // delay in multiples of 1ms
//---------------------------------------------------------------------
void RGB(uint8_t Red,uint8_t Green,uint8_t Blue); // RGB-LED Control: 1=on, 0=off, for each of the 3 colors
// *** MAIN *********************************************************
//-------------------------------------------------------------------
int main(void)
{
MCU_Init(); // MCU Initialization; has to be done prior to anything else
RGB(0,0,0); // Start with all LEDs off
__asm("CPSIE i"); // Enable all Interrupts
NVIC->ICPR[0] = (uint32_t)(1 << (LLWU_IRQn & 0x1F)); // Clear LLUW Interrupt in NVIC Core register
NVIC->ISER[0] = (uint32_t)(1 << (LLWU_IRQn & 0x1F)); // Set LLUW Interrupt in NVIC Core register
volatile int dummyread;
// Allow any of the Low-Leakage Stop modes.
SMC_PMPROT = SMC_PMPROT_ALLS_MASK;
// Allow entry into the Low-Leakage Stop (LLS) mode.
SMC_PMCTRL = SMC_PMCTRL_STOPM(3);
// Enable hi to lo transition for LLWU_P6 / pin-C1.
LLWU_PE2 = 0x20;
// Set the SLEEPDEEP bit to enable deep sleep mode.
// (W/o this we only drop to about 3.1mA down from 4.6mA.)
SCB->SCR |= SCB_SCR_SLEEPDEEP_Msk;
for(;;)
{
__asm("WFI"); // Enter low power mode
dummyread = PMC_REGSC;
RGB(1,0,0); // Turn on RED LED
MCU_Delay(200); // Delay 200ms
RGB(0,0,0);
}
}
//-------------------------------------------------------------------
// ******************************************************************
// FUNCTION BODIES //////////////////////////////////////////////////
//-------------------------------------------------------------------
void MCU_Init(void)
{
// Crucial
__asm("CPSID i"); // Disable interrupts
//Disable Watchdog
SIM_COPC=0x00; // Disable COP watchdog
//System Registers
SIM_SCGC5|=SIM_SCGC5_PORTA_MASK; // Enable PortA clock
SIM_SCGC5|=SIM_SCGC5_PORTB_MASK; // Enable PortB clock
SIM_SCGC5|=SIM_SCGC5_PORTC_MASK; // Enable PortC clock
SIM_SCGC5|=SIM_SCGC5_PORTD_MASK; // Enable PortD clock
SIM_SCGC5|=SIM_SCGC5_PORTE_MASK; // Enable PortE clock
// System clock initialization
MCG_MC|=MCG_MC_HIRCEN_MASK; // Enable 48MHz HIRC
MCG_C1=MCG_C1_CLKS(0); // Enable Main Clock Source of the 48MHz HIRC
SIM_CLKDIV1&=~(SIM_CLKDIV1_OUTDIV1(1)); // Set Core Clock/1=48MHz
SIM_CLKDIV1|=(SIM_CLKDIV1_OUTDIV4(1)); // Set Bus Clock/2=24MHz
// System Tick Init
SysTick->CTRL=0; // Disable the SysTick Timer
SysTick->LOAD=48000; // Core Clock/1=48MHz, Period=1ms/(1/48000000Hz)=48000
SysTick->VAL=0; // Clear the current counter value to 0
SysTick->CTRL=(SysTick_CTRL_ENABLE_Msk
|SysTick_CTRL_CLKSOURCE_Msk); // Enable SYS TICK timer and set clock source to processor clock (core clock)
// GPIO Init
PORTC->PCR[1] |= PORT_PCR_MUX(1)| // Enable Port Pin PTC1 as GPIO
PORT_PCR_PE_MASK| // Select the resistor to pull up or down on port pin
PORT_PCR_PS_MASK| // Select a pull up resistor
PORT_PCR_IRQC(0x08); // Configure interrupt pin to trigger on a logic low (0)
GPIOC->PDDR&=~(1<<1); // make sure GPIO PTC1 pin is configured as an input
PORTB_PCR18=PORT_PCR_MUX(1); // Set Pin B18 to GPIO function
PORTB_PCR19=PORT_PCR_MUX(1); // Set Pin B19 to GPIO function
PORTA_PCR13=PORT_PCR_MUX(1); // Set Pin A13 to GPIO function
GPIOB_PDDR|=(1<<18); // Set Pin B18 as output
GPIOB_PDDR|=(1<<19); // Set Pin B19 as output
GPIOA_PDDR|=(1<<13); // Set Pin A13 as output
}
//---------------------------------------------------------------------
void MCU_Delay (uint32_t delay) // Delay in multiples of 1ms (e.g. use 1000 for 1 second)
{
uint32_t delw;
for (delw=0;delw<delay;delw++)
{
while (!(SysTick->CTRL&SysTick_CTRL_COUNTFLAG_Msk));
}
}
//---------------------------------------------------------------------
void RGB(uint8_t Red,uint8_t Green,uint8_t Blue) // RGB-LED Control: 1=on, 0=off, for each of the 3 colors
{
if (Red ==1) GPIOB_PCOR|=(1<<18); else GPIOB_PSOR|=(1<<18);
if (Green ==1) GPIOB_PCOR|=(1<<19); else GPIOB_PSOR|=(1<<19);
if (Blue ==1) GPIOA_PCOR|=(1<<13); else GPIOA_PSOR|=(1<<13);
}
//---------------------------------------------------------------------
// INTERRUPT BODIES /////////////////////////////////////////////////
//-------------------------------------------------------------------
void LLWU_IRQHandler (void)
{
// Clear WUF6 (aka LLWU_P6) by writing a 1 to the flag bit.
LLWU_F1 = 0x40; // Clear interrupt flag
RGB(0,0,1); // Turn on BLUE LED
MCU_Delay(200); // Delay 200ms
RGB(0,0,0);
}
// code end
Hi Rick
Glad to hear you solved it.
Do you by any chance have a circuit diagram to the FRDM-KL27Z?
I haven't been able to find one (???)
Regards
Mark
I asked. There are some bits of the FRDM-KL27Z schematic in the user's guide. I think someone is going to look into the whole schematic.
> That is odd - I'll see what I can do.