Use of 6 channels of FTM on MKE02Z32

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Use of 6 channels of FTM on MKE02Z32

485件の閲覧回数
rpflaum
Contributor II

I am looking to use the 6 channel Flex Timer Module on a KE02Z32 using Processor Expert. However when I add the FTM component to my design I am only seeing 2 channels available. Does Processor Expert handle the 6 channel FTM? If so how do I access it?

ラベル(1)
0 件の賞賛
1 返信

366件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Robert Pflaum,

    Please check which FTM module you are using?

pastedImage_1.png

From the above picture, you can find FTM0 and FTM1 only have 2 channels, so, if you want to use 6 FTM channels, you need to select the FTM2 module.

Wish it helps you!

If you still have question, please let me know!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------