Trigger ADC with PDB from eFlexPWM - KV44F256x

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Trigger ADC with PDB from eFlexPWM - KV44F256x

Jump to solution
551 Views
katha
Contributor II

Hello,

is there an example code of how to trigger ADC via PDB from eFlexPWM with a KV44F256x?

Is there a possibility to get Peripherals tool for KV44F256x?

(code example for eFlexPWM for KV44F256x like in AN4410)

Regards

Katharina

Labels (1)
0 Kudos
1 Solution
452 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Katharina,

 

You can take as reference the following application note. I believe it may be helpful for you.

https://www.nxp.com/docs/en/application-note/AN5237.pdf 


Have a great day,
Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
1 Reply
453 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Katharina,

 

You can take as reference the following application note. I believe it may be helpful for you.

https://www.nxp.com/docs/en/application-note/AN5237.pdf 


Have a great day,
Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos