Hi,
Is there any available eGUI project that can be used to drive the 4.3'' LCD display on the TWR-K70F120 using KDS?
I used to be able to run the eGUI but now I get Error: Program "make" not found in PATH.
Not sure what it is because it has been a while since I used this, but though might be worth starting with a fresh new up to date project.
Thanks,
Ylber
Hi Ylber,
Unfortunately, we don't have TWR-K70F120M and TWR-LCD-RGB with eGUI software based on KDS software.
Please check attached eGUI software for IAR software based on TWR-K70F120M and TWR-LCD-RGB boards.
Wish it helps.
Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
Porcessor Expert provides LDCD_LDD component, you can configure it to fit your needs.
LCDC_LDD provides general API for LCD controllers. The component provides standard features (if supported by hardware) and also special functions provided by the hardware:
Passive monochrome or color panels (CSTN)
TFT panels
Standard panel interface (1, 2, 4, 8, 12, 16, 18, 24 bit bus width)
Standard synchronization signals
Self-refresh mode
PWM contrast control
Hardware cursor
Hardware alpha blending
Hardware color keying
Multiple planes
The LCDC_LDD component provides typical usage example at component help content.
Customer could refer it.
Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
Thanks very much. I have added the LCDC_LDD from processor expert to the K70, but when I try to add the UserInterface errors pop up because the list processor expert gives me contains LCD controllers that I do not use. How can I add and configure the UserInterface component for the TWR-LCD-RGB?
Kind Regards,
Ylber