The USB CDC Virtual COM demo (cdc_vcom_twrk40x256) that ships with MQX 3.7 stops working (device will not enumerate) as soon as MQX 3.7 is updated to use the Processor Expert Logical Level Device Driver enabled BSP (bsp_twrk40x256_pe) instead of the default BSP (bsp_twrk40x256).
My configuration:
Operating System: Windows XP SP2
IDE: CodeWarrior 10.1
RTOS: MQX 3.7
After a clean installation of CW 10.1 and MQX 3.7...
Steps to reproduce USB CDC device enumeration problem:
I did a clean build of all MQX libs and the device will still not enumerate.
bsp_twrk40x256_pe
psp_twrk40x256
mfs_twrk40x256
rtcs_twrk40x256
shell_twrk40x256
usb_ddk_twrk40x256
usb_hdk_twrk40x256
Any ideas?
解決済! 解決策の投稿を見る。
See the following posting for the solution:
This may or may or may not be related, but I am having problems with opening serial ports between simple terminal apps like TeraTerm and a C# windows program that utilizes the Serial Port API within Visual Studio.
I've tracked this problem down to code in the top part of USB_Notif_Callback. This start_transactions variable only gets set if there is an event_type = 24 (USB_APP_CDC_DTE_ACTIVATED). Although this makes good sense, opening up a port in Visual Studio sends a sequence (three times) of 22, 23. (USB_APP_CDC_CARRIER_ACTIVATED), (USB_APP_CDC_DTE_DEACTIVATED). If event_type = 24 is never sent, then the port will stall on attempting to write a character, and then throw an exception if any additional characters are send after the first.
void USB_Notif_Callback(uint_8 event_type,void* val,pointer arg)
{
uint_32 handle;
uint_8 index;
handle = *((uint_32 *)arg);
if(start_app == TRUE)
{
if(event_type == USB_APP_CDC_DTE_ACTIVATED)
{
start_transactions = TRUE;
}
...
Using TeraTerm, when opeing up a COM port sends 22 (USB_APP_CDC_CARRIER_ACTIVATED) ,24 (USB_APP_CDC_DTE_ACTIVATED), which makes good sense. So this appears to be a limitation of Visual Studio. I'm looking into how to change this behavior if at all possible within the serial windows driver.
I know this post is 4.5 years old but did you ever find a solution? I am having the exact same issue.
Verify the USB clock frequency in the CPU component. See" CPU component \ Clock configurations \ Clock configuration 0 \ System clocks \ PLLFLL clock selection \ USB clock settings \ USB clock". USB module requires 48 MHz clock . .
The clock settings are set correctly. Seet attached screenshot of my settings. I did not modify these settings at all after a clean install of MQX 3.7, which means the settings in my screenshot represent the settings that ship with MQX 3.7.
I contacted a Freescale rep. and received the following as the reply:
"Have Robotronics run the demo file in C:\Program Files\Freescale\Freescale MQX 3.7\usb\device\examples\cdc\virtual_com\cw10 When run, they will be asked to install a .inf file for the CDC. It’s in C:\Program Files\Freescale\Freescale MQX 3.7\usb\device\examples\cdc\virtual_com\inf Run both the P&E Terminal Program (which reports status) and open a terminal program (Hyperterm, PuTTY, TerraTerm) using the COM port assigned by Windows."
The P&E Terminal is not necessary to successfully run the CDC demo (cdc_vcom_twr40x256) using the default BSP and
attaching the P&E Terminal to the USB COM to monitor status didn't help solve the problem when using the Processor Expert enabled BSP. The P&E Terminal reported no status while flashing the processor or when attempting to enumerate the tower module as a CDC USB device.