TSI KE15 INDEPENDENT CH CONFIG

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

TSI KE15 INDEPENDENT CH CONFIG

1,312 次查看
Macgayver
Contributor I

Hi !

I'm using tsi_v5 and MKE15 uC.

 

Is possible configure hardware parameters for each TSI channel independently ?:

    userConfig->commonConfig.mainClock = kTSI_MainClockSlection_0;

    userConfig->commonConfig.mode = kTSI_SensingModeSlection_Self;

    userConfig->commonConfig.dvolt = kTSI_DvoltOption_2; 

...   

userConfig->chargeCurrent = kTSI_CurrentMultipleChargeValue_1;

//

or it configs for all TSI Channels the same parameters?

 

my understand is that Init TSI function initializes all TSI channels with same features, can someone confirm ?

 // Initialize the TSI
TSI_InitSelfCapMode(TSI, &userConfig);  

 

tks

0 项奖励
回复
1 回复

1,304 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Macgayver,

Your assumption is correct, the TSI driver initialization function configures all TSI channels with the same parameters. There are no individual configuration registers to allow each channel to have independent parameters.

I you haven’t read it I would recommend Application Note 3863 (AN3863, link below) which covers recommendations when using touch sensing electrodes.

https://www.nxp.com/docs/en/application-note/AN3863.pdf

I hope that this information helps!

Regards,
Gustavo

0 项奖励
回复