TRK-KEA8 project build problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TRK-KEA8 project build problem

Jump to solution
1,756 Views
lim
Contributor II

Hi NXP

 

I just try to build  EEPROM emulation driver for KEA128 and KEA8 project at the Code Warrior 
but when i import project, problem has occurred

I think this problem is caused by not installing the right software. I couldn't find a right codewarrior installing software

please can i have download link ? and do you have any idea about that problem?

product : TRK-KEA8

project : EEPROM emulation driver for KEA128 and KEA8

 

error detail

An error has occurred. see error log for more details.
Would you like to export diagnostic information and send it to freescale?
Unknown target type : com.freescale.cwsystem.kinetis.KAZN.KEAZN8M4
 
0 Kudos
1 Solution
1,708 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi lim,

Sorry for my last reply!
According to the error message, seems that you did not choose Kinetis when install the CodeWarrior.

Choose Components.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

5 Replies
1,745 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi lim,

Please try to copy and paste the folder KEA_SGF180 to a place.
And then import the example: KEA_SGF180\Demos\build\TRK_KEAZN8\cw
I am able to build it by using CodeWarrior11.1.

Import Projects.pngbuild.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
1,736 Views
lim
Contributor II

Thank you for replying Robin

 

I just try build a project like your last message 

but when import a project, problem has occurred like first picture

do you have any idea about that problem?

 

Code warrior ver. 11.1

Thank you

0 Kudos
1,709 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi lim,

Sorry for my last reply!
According to the error message, seems that you did not choose Kinetis when install the CodeWarrior.

Choose Components.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

1,689 Views
lim
Contributor II

Thank you i solved that problem 

 

Thank you very much

1,699 Views
lim
Contributor II

Thank you very much Robbin i solve that problem

but still can not build a project  

 

 

0 Kudos