Securing flash of MCU-MKV46F256xxx16

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Securing flash of MCU-MKV46F256xxx16

413 Views
reshma-nexgen
Contributor I

Hi,

I'm using MKV46F256xxx16 in my project and I want to secure the MCU. After I secure the MCU, the MCU code is not working.

I have changed the flash configuration bit in startup_mkv46f16.c. as follows:

reshmanexgen_0-1658740287830.png

Here “F8” represents the following configurations:

  • KEYEN : 11 Backdoor key access disabled
  • MEEN: 11 Mass erase is enabled
  • FSLACC: 10 NXP factory access denied
  • SEC: 00 MCU security status is secure.

I have also selected "allow security" in JLink Debugger section.

reshmanexgen_1-1658740391505.png

After I secure the MCU the code is not working. Attached is the test program. In here, PORTB pin 2 is toggles at ~7KHz. After securing the MCU, this toggling is not observed even after power recycle.

 

Let me know if there is a way to solve this issue.

Regards,

Reshma.

Labels (1)
0 Kudos
1 Reply

394 Views
PabloAvalos
NXP TechSupport
NXP TechSupport

Hi @reshma-nexgen 

 

Thanks a lot for reaching our technical support and thanks for your patience.

 

Regarding your issue, you mean that before securing your mcu, you were able to see that pin toggling @7 KHz ? Confirming this, it is supposed that for securing the mcu you only need to modify the SEC register, depending on the security you want. You may refer to this application note for reference: https://www.nxp.com/docs/en/application-note/AN4507.pdf 

 

Hope the information was helpful, please let me know if you have some more questions or comments.

 

Sincerely,
Pablo Avalos.

0 Kudos