Hello,
I am looking fot SDHC library for my kinetis k60.
I use IAR and I would like to be able to write information on SD card.
Is there any SDHC library already develop?
Best regard.
Hello Xavier:
Those are good suggestions by Luciano and Mark. For the case of KSDK, you can find a document about using the SDHC driver in the next link:
FatFs + SDHC data logger with KSDK in Kinetis Design Studio
Regards!
Jorge Gonzalez
Hi Xavier
You can also try utFAT - http://www.utasker.com/docs/uTasker/uTasker_utFAT.PDF
This has more features that FatFS, including data caching between shared files, file analysis functions, undelete, as well as FAT emulation - http://www.utasker.com/docs/uTasker/uTaskerEmulatedFAT.pdf
Works with all Kinetis parts (with SPI or SDHC) and all common IDEs (IAR, Keil, KDS, CW, Atollic, Green Hills, Rowley, CooCox, etc.) and allows SDHC/SD card simulation in VisualStudio.
http://www.utasker.com/forum/index.php?topic=1667.0
Supports multiple disks (SD card, Memory Sticks, multiple USB-MSD LUMs).
Regards
Mark
If you're using MQX the MFS library works well. I've used it on multiple boards for reading USB and SDHC filesystems. Otherwise, under the KSDK there is also the FatFS drivers. I haven't used them myself, but they should work for your purpose.