Hi,
I'm using k70 Tower kit with resistive touch twr-lcd module.
I'm using bare metal project.
Can anyone share some sample code for resistive touch twr-lcd(for k70).
Regards
Ankur
Hello,
You can also check the eGUI code. It includes drivers for resistive touch screen and ADC.
https://github.com/Gargy007/eGUI/tree/master/D4D/low_level_drivers/touch_screen
This is the configyration for TWR-K70 using the TWR-LCD touch screen. Notice, you need hardware rework to connect resistive touch in TWR-LCD to TWR-K70.
#define D4DTCH_ADC_HW D4DTCH_ADC_HW_KINETIS
#define D4DTCH_ADC_ID 1 // Use ADC module 1
#define D4DTCH_MCU_USER_INIT {D4DTCH_X_PLUS_PCR = PORT_PCR_MUX(1) | PORT_PCR_DSE_MASK;\
D4DTCH_X_MINUS_PCR = PORT_PCR_MUX(1) | PORT_PCR_DSE_MASK;\
D4DTCH_Y_PLUS_PCR = PORT_PCR_MUX(1) | PORT_PCR_DSE_MASK;\
D4DTCH_Y_MINUS_PCR = PORT_PCR_MUX(1) | PORT_PCR_DSE_MASK;\
}
// X+ wire definition
#define D4DTCH_X_PLUS 17
#define D4DTCH_X_PLUS_PORT GPIOA_PDOR // Data output register
#define D4DTCH_X_PLUS_DDR GPIOA_PDDR // Output enable register
#define D4DTCH_X_PLUS_ADCH 17 // ADC channel number
#define D4DTCH_X_PLUS_PCR PORTA_PCR17
// X- wire definition
#define D4DTCH_X_MINUS 10
#define D4DTCH_X_MINUS_PORT GPIOB_PDOR
#define D4DTCH_X_MINUS_DDR GPIOB_PDDR
#define D4DTCH_X_MINUS_PCR PORTB_PCR10
// Y+ wire definition
#define D4DTCH_Y_PLUS 6
#define D4DTCH_Y_PLUS_PORT GPIOB_PDOR
#define D4DTCH_Y_PLUS_DDR GPIOB_PDDR
#define D4DTCH_Y_PLUS_ADCH 12
#define D4DTCH_Y_PLUS_PCR PORTB_PCR6
//#define D4DTCH_INIT_Y_PLUS OUTPUT(D4DTCH_Y_PLUS); RESET(D4DTCH_Y_PLUS);
//#define D4DTCH_RESET_Y_PLUS RESET(D4DTCH_Y_PLUS);
//#define D4DTCH_SET_Y_PLUS SET(D4DTCH_Y_PLUS);
// Y- wire definition
#define D4DTCH_Y_MINUS 5
#define D4DTCH_Y_MINUS_PORT GPIOB_PDOR
#define D4DTCH_Y_MINUS_DDR GPIOB_PDDR
#define D4DTCH_Y_MINUS_PCR PORTB_PCR5
//#define D4DTCH_CALIB_CROSS_OFFSET 30
// Constant specifying maximum ADC value for a screen touch (=12bits)
#define D4DTCH_FULL_SCALE 0x0FFF
// Constants specifying minimum ADC value for a screen touch
#define D4DTCH_X_TOUCH_MIN (D4DTCH_FULL_SCALE / 10)
#define D4DTCH_Y_TOUCH_MIN (D4DTCH_FULL_SCALE / 10)
#define D4DTCH_X_TOUCH_OFFMAX (D4DTCH_X_TOUCH_MIN * 3)
#define D4DTCH_Y_TOUCH_OFFMAX (D4DTCH_Y_TOUCH_MIN * 3)
// Constants specifying ADC difference for touch screen sample
//#define D4DTCH_SAMPLE_MARGIN (D4DTCH_FULL_SCALE / 256)
Hi Luis,
Thanks for reply.
This D4D project is expecting "mqx.h" file.
But I'm not using MQX ,my project is bare board project(using codewarrior 10.6.4).
Should I download MQX and integrate it with CW or without MQX it's possible to configure and use "touch twr-lcd"??
if I have need MQX then which version of it??
Regards
Ankur
Hi Ankur,
eGUI (D4D) can work also in bare metal. Notice that TWR-K70 is used together with TWR-LCD-RGB. In this case, touch is controlled by CRTOUCH device populated in the TWR-LCD-RGB. So, all the examples you will find are based on TWR-K70 + TWR-LCD-RGB (using LCDC K70 module and CRTOUCH). http://www.freescale.com/products/sensors/touch-sensors/freescale-touch-sensing-platform-a-ready-pla...
But the configuration I gave you is coming from old demo using TWR-K70 + TWR-LCD where LCD was controlled by K70 Flexbus and touch using K70 ADC channels. But hardware rework was required because the TWR-K70 ADC channels connected to TWR-LCD doesn't have GPIO capability, as you know, that is needed for implementing a touch sensing with ADC/GPIO.
Luis
Hi
See http://www.utasker.com/docs/uTasker/uTaskerTouch.PDF
Code for K70 and TWR-LCD is included in the uTasker project at http://www.utasker.com/forum/index.php?topic=1721.0
Search for SUPPORT_TOUCH_SCREEN in the code and the settings for K70F150M_12M.
Initialisation is fnStartTouch() in glcd_tft.h and the interrupt is handled in fnTouchInterrupt().
The touch operation is also simulated in the uTasker Kinetis simulator - as show in screen shot below:
Video of the operation: https://www.youtube.com/watch?v=PvsFFRigwFU (same operation on TWR-K70)
Regards
Mark
Kinetis: http://www.utasker.com/kinetis.html
K70: http://www.utasker.com/kinetis/TWR-K70F120M.html / http://www.utasker.com/kinetis/EMCRAFT_K70F120M.html
For the complete "out-of-the-box" Kinetis experience and faster time to market