Problem with OM2385/FS001 which launches "Demo_55.2MHz.s19" file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem with OM2385/FS001 which launches "Demo_55.2MHz.s19" file

712 Views
yogaCHEN
Contributor I

I am using OM2385/FS001 development kit for research, but after dropping the microcode file SF_KL43Z_OL2385_Demo_55.2MHz.s19 onto the FRDM-KL43Z icon on the host PC and turning on the board, it will report error on the terminal emulator, as shown below:

yogaCHEN_0-1634131294980.png

And I check the demo project SF_KL43Z_OL2385_Demo download from Embedded SW for SIGFOX Based on OL2385 ,  find that the ACK frame return the error code sfErrUnknownSpiCommand after sending change network standard command, as shown below:

yogaCHEN_1-1634132253992.png

The problem confused me a lot, could somebody teach me how to launch correct microcode file and run the board successfully.

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

655 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @yogaCHEN,

What is the module version that you are working on?

Could you please comment on the line SetupSigfoxDriver? The Set up is sending a new command that the previous versions do not support.

Please let me know your findings.

Regards,

Mario

0 Kudos
Reply