Problem with OM2385/FS001 which launches "Demo_55.2MHz.s19" file

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problem with OM2385/FS001 which launches "Demo_55.2MHz.s19" file

713 次查看
yogaCHEN
Contributor I

I am using OM2385/FS001 development kit for research, but after dropping the microcode file SF_KL43Z_OL2385_Demo_55.2MHz.s19 onto the FRDM-KL43Z icon on the host PC and turning on the board, it will report error on the terminal emulator, as shown below:

yogaCHEN_0-1634131294980.png

And I check the demo project SF_KL43Z_OL2385_Demo download from Embedded SW for SIGFOX Based on OL2385 ,  find that the ACK frame return the error code sfErrUnknownSpiCommand after sending change network standard command, as shown below:

yogaCHEN_1-1634132253992.png

The problem confused me a lot, could somebody teach me how to launch correct microcode file and run the board successfully.

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

656 次查看
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @yogaCHEN,

What is the module version that you are working on?

Could you please comment on the line SetupSigfoxDriver? The Set up is sending a new command that the previous versions do not support.

Please let me know your findings.

Regards,

Mario

0 项奖励
回复