Hi.
I used with TWR-K60 board for develop my project. All SW modules already finished and now I need to move project platform to K61 MCU (this MCU will work in final board). In this project I used with LCD that allowed in LCD demo board, HID keyboard host project (use USB keyboard), I2C, UART, timers and I need to configure K61 MCU for correct work operation of my system.
Can I use with this configuration for K61 without any another changes (in timers configuration, for example, or in LCD, USB HID use). Can I use with CPU function for 100us delay (in Processor Expert for k61 I don't view this function) or I need to configure all peripheries from the beginning?
For K60 MCU configuration I used two function (as in keyboard_host project for TWR-K60):
void MCU_Init(void)
{
// Point the VTOR to the new copy of the vector table
SCB_VTOR = (uint_32)___VECTOR_RAM;
//Clear any pending interrupts on USB
NVICICER2|=(1<<9);
//Enable interrupts from USB module
NVICISER2|=(1<<9);
// init pll
PLL_Init();
// SIM Configuration
MPU_CESR=0;
// USB Clock Gating
SIM_SCGC4|=(SIM_SCGC4_USBOTG_MASK);
// PLL/FLL selected as CLK source
SIM_SOPT2 |= SIM_SOPT2_USBSRC_MASK | SIM_SOPT2_PLLFLLSEL_MASK;
// USB Freq Divider
SIM_CLKDIV2=0x02;
// weak pulldowns
USB0_USBCTRL=0x40;
}
and
*****************************************************************************
* It will configure the MCU to disable STOP and COP Modules.
* It also set the MCG configuration and bus clock frequency.
****************************************************************************/
static void PLL_Init()
{
// First move to FBE mode
// Enable all of the port clocks. These have to be enabled to configure pin muxing options, so most code will need all of these on anyway.
SIM_SCGC5 |= (SIM_SCGC5_PORTA_MASK
| SIM_SCGC5_PORTB_MASK
| SIM_SCGC5_PORTC_MASK
| SIM_SCGC5_PORTD_MASK
| SIM_SCGC5_PORTE_MASK );
#ifdef MCU_MK60N512VMD100
// Enable external oscillator, RANGE=0, HGO=, EREFS=, LP=, IRCS=
MCG_C2 = 0;
#else
// Enable external oscillator, RANGE=2, HGO=1, EREFS=1, LP=0, IRCS=0
MCG_C2 = MCG_C2_RANGE(2) | MCG_C2_HGO_MASK | MCG_C2_EREFS_MASK|MCG_C2_IRCS_MASK;
#endif
// Select external oscillator and Reference Divider and clear IREFS to start ext osc
// CLKS=2, FRDIV=3, IREFS=0, IRCLKEN=0, IREFSTEN=0
MCG_C1 = MCG_C1_CLKS(2) | MCG_C1_FRDIV(3);
#ifndef MCU_MK60N512VMD100
// wait for oscillator to initialize
while (!(MCG_S & MCG_S_OSCINIT_MASK)){};
#endif
// Wait for Reference clock Status bit to clear
while (MCG_S & MCG_S_IREFST_MASK){};
// Wait for clock status bits to show clock source is ext ref clk
while (((MCG_S & MCG_S_CLKST_MASK) >> MCG_S_CLKST_SHIFT) != 0x2){};
#ifdef MCU_MK60N512VMD100
MCG_C5 = MCG_C5_PRDIV(BSP_REF_CLOCK_DIV - 1);
#else
MCG_C5 = MCG_C5_PRDIV(BSP_REF_CLOCK_DIV - 1) | MCG_C5_PLLCLKEN_MASK;
#endif
// Ensure MCG_C6 is at the reset default of 0. LOLIE disabled, PLL enabled, clk monitor disabled, PLL VCO divider is clear
MCG_C6 = 0;
// Set system options dividers
SIM_CLKDIV1 = SIM_CLKDIV1_OUTDIV1(BSP_CORE_DIV - 1) | // core/system clock
SIM_CLKDIV1_OUTDIV2(BSP_BUS_DIV - 1) | // peripheral clock;
SIM_CLKDIV1_OUTDIV3(BSP_FLEXBUS_DIV - 1) | // FlexBus clock driven to the external pin (FB_CLK)
SIM_CLKDIV1_OUTDIV4(BSP_FLASH_DIV - 1); // flash clock
// Set the VCO divider and enable the PLL, LOLIE = 0, PLLS = 1, CME = 0, VDIV
MCG_C6 = MCG_C6_PLLS_MASK | MCG_C6_VDIV(BSP_CLOCK_MUL - 24); // 2MHz * BSP_CLOCK_MUL
// wait for PLL status bit to set
while (!(MCG_S & MCG_S_PLLST_MASK)){};
// Wait for LOCK bit to set
while (!(MCG_S & MCG_S_LOCK_MASK)){};
// Transition into PEE by setting CLKS to 0
// CLKS=0, FRDIV=3, IREFS=0, IRCLKEN=0, IREFSTEN=0
MCG_C1 &= ~MCG_C1_CLKS_MASK;
// Wait for clock status bits to update
while (((MCG_S & MCG_S_CLKST_MASK) >> MCG_S_CLKST_SHIFT) != 0x3){};
//return 0;
} //pll_init
Thanks.
Evgeni.
解決済! 解決策の投稿を見る。
Hello,
this is not exaclty the same thing as delay 100us function, but you might use this one:
http://www.steinerberg.com/EmbeddedComponents/Wait
I use it instead of the Delay100us() with Kinetis.
Hope this helps.
BK
Hello,
the 100us delay function is not supported on any Kinetis MCU. However there could be no problem in migration of ProcessorExeprt project from K60 -> K61.
best regards
Vojtech Filip
Processor Expert Support Team
Hello,
this is not exaclty the same thing as delay 100us function, but you might use this one:
http://www.steinerberg.com/EmbeddedComponents/Wait
I use it instead of the Delay100us() with Kinetis.
Hope this helps.
BK
Thanks