MKL15Z128VFM4 LLWU wakeup pin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MKL15Z128VFM4 LLWU wakeup pin

1,607件の閲覧回数
geniusgogo
Contributor I

my board used LPTMR and PTC3 wakeup the LLWU mode on VLPS,

LPTMR able wakeup,

PTC3 can't wakeup,

What causes it?

init code:

llwu_external_pin_filter_mode_t filterMode;

pin_config.pinDirection = kGPIO_DigitalInput;
pin_config.outputLogic = 0;

// MCU wakeup pin
GPIO_PinInit(GPIOC, 3, &pin_config);

/* Setup LPTMR. */
LPTMR_GetDefaultConfig(&lptmrConfig);
lptmrConfig.prescalerClockSource = kLPTMR_PrescalerClock_1; /* Use LPO as clock source. */
lptmrConfig.bypassPrescaler = true;
lptmrConfig.enableFreeRunning = true;
LPTMR_Init(LPTMR0, &lptmrConfig);
LPTMR_EnableInterrupts(LPTMR0, kLPTMR_TimerInterruptEnable);
LLWU_EnableInternalModuleInterruptWakup(LLWU, 0, true);
// setup external PTC3 pin
LLWU_SetExternalWakeupPinMode(LLWU, 7, kLLWU_ExternalPinAnyEdge);
NVIC_EnableIRQ(LLWU_IRQn);
NVIC_EnableIRQ(LPTMR0_IRQn);

......

sleep ongo:

LPTMR_SetTimerPeriod(LPTMR0, 60000);
LPTMR_StartTimer(LPTMR0);
LLWU_SetExternalWakeupPinMode(LLWU, 7, kLLWU_ExternalPinAnyEdge);
SMC_SetPowerModeVlps(SMC);

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

982件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi genius gogo

If you want to set LLS mode you could check the following doc:https://community.nxp.com/docs/DOC-332687 

Here is an example of how to set and use this mode in a FRDM-KL26Z.

Hope this could help

Regards

Jorge Alcala

0 件の賞賛
返信

982件の閲覧回数
mjbcswitzerland
Specialist V

Hi

The LLUW can't be used to wake the processor from VLPS (very low power STOP) because this mode is not a Low Leakage Mode (from LLS), meaning that the LLWU is not active when you set the VLPS mode.
To wake from VLPS you need an asynchronous interrupt. You can wake if you set LLS, for example.

http://www.utasker.com/kinetis/LLWU.html

Regards

Mark

http://www.utasker.com/kinetis/FRDM-KL25Z.html

0 件の賞賛
返信

982件の閲覧回数
geniusgogo
Contributor I

thanks,really is so.

very very thanks.

0 件の賞賛
返信