Hello. I'm developing a project with MKL05. This project should be powered with four AA batteries and almentar the useful life of the battery I have to put the PC to sleep (low power) and waking through TSI. Can anyone help me. I got an example of the KL25 that does the same, but when the system calls the function "GotoLowPower ()", the micro sleeps and does not wake up more. It is caught in the "DO WHILE".
Thank you.
已解决! 转到解答。
Hello Paul, follows the code I am using as an example. From it I will develop my application.
I will be very grateful if you can help me.
If you are not able to download the file let me know that I command again.
Thank you.
Hi Eliezer
The KL05 has an errata about the TSI and the LPTMR, please check it ERRATA 6060 TSI: Out of Range interrupt shows incorrect behavior with some configurations on the following link:
Because of this is better use the LPTMR to wake up the MCU check if there is any touch and then go to stop again, please check the attached project, this is for the freedom kl05 and use one electrode, if the electrode is not touch for some time the MCU goes to LLS and is waking up periodically to check if there is a touch or not,.
I hope this will help you.
Regards
Vicente
Hello Paul, follows the code I am using as an example. From it I will develop my application.
I will be very grateful if you can help me.
If you are not able to download the file let me know that I command again.
Thank you.