MKE06Z64VLD4 PTB0 and PTB1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MKE06Z64VLD4 PTB0 and PTB1

709件の閲覧回数
RBORB
NXP Employee
NXP Employee

Hello,

Looking at the data sheet and reference manual pinout for the MK06 44 pin LQFP PTB0 is assigned to pin 24 and PTB1 is assigned to pin 23.  But ProcessorExpert shows the pins flipped i.e. PTB0 = pin 23 and PTB1 = Pin24.  Which is correct?

Thx,

Ronen

ラベル(1)
0 件の賞賛
2 返答(返信)

448件の閲覧回数
william_jiang
NXP Apps Support
NXP Apps Support

Hi All,

That is diagram issue for the position of these two pins on 44LQFP package in data sheet and reference manual.

That is, PTB1 is on pin 23, PTB0 is on pin 24.

The issue is fixed in new version to be published. Thanks.

0 件の賞賛

447件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Ronen,

I am using ProcessorExpert in KDS3.2.0, this version seems correct.

You can try to update the software.

Installation Details.jpg

PTB0 Pin24 MKE06Z64VLD4.jpgPTB1 Pin23 MKE06Z64VLD4.jpg

Best Regards,

Robin

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛