I have a problem and want to see if you can help me.
I'm trying to record a Kinetis uControlador Freescale, the MKE04Z8VWJ4 but am not having success ...
I'm using the recorder "Multilink Universal", green model.
Following existing development models, connected pins "SWD_DIO, SWD_CLK, Reset, + 5V and GND" to the burner pins.
However the time of recording, it generates error.
Is there any limitation on the recorder with the microcontroller model?
已解决! 转到解答。
It can be used, but you will have to make sure nothing attached to it is pulling the pin low until the NMI can be disabled. The SIM module has the registers to control the NMI function. If you're using Processor Expert, it can be disabled through that.
Hi,
The P&E USB Multilink Universal tool provides below Kinetis debug port:
I checked your attached debugger interface, there without problem.
The NMI pin is default to NMI function after the MCU POR, and there with internal pullup device enabled when NMI is enabled.
When there with low voltage detected at NMI pin, the NMI related Non-maskable interrupt will be triggered with Vector2 at ARM's NVIC.
Have a great day,
best regards,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
this one shows how to map the NMI as GPIO pin with Processor Expert:
It can be used, but you will have to make sure nothing attached to it is pulling the pin low until the NMI can be disabled. The SIM module has the registers to control the NMI function. If you're using Processor Expert, it can be disabled through that.