Hi everyone,
I am facing problems in implementing the SPI module in MKE04Z128VLK4 chip. I initialzed the chip for the following conditions.
/*
* masterConfig->enableStopInWaitMode = false;
* masterConfig->polarity = kSPI_ClockPolarityActiveHigh;
* masterConfig->phase = kSPI_ClockPhaseFirstEdge;
* masterConfig->direction = kSPI_LsbFirst ;
* masterConfig->dataMode = kSPI_8BitMode;
* masterConfig->txWatermark = kSPI_TxFifoOneHalfEmpty;
* masterConfig->rxWatermark = kSPI_RxFifoOneHalfFull;
* masterConfig->pinMode = kSPI_PinModeOutput;
* masterConfig->outputMode = kSPI_SlaveSelectAutomaticOutput;
* masterConfig->baudRate_Bps = 500000U;
*/
The regsiter values are C1 = 0xF3, C2 = 0x19, BR = 0x00;
Chip select pin is high after initializing SPI but does not go low after data is moved to Data register.
The code is entering the ISR but I do not see any output on the pins of CLK or MOSI.
I am also multiplexing the SPI pins initially. I attached my full project.
Thanks,
Hi Shoaib Shaikh,
I try to flash your code into FRDM-KE06Z board.
I do see output on the pins of PTG4(CLK) and PTG5(MOSI).
Due to the PTG5~PTG7 are connect to LEDs, so I only connect the PTG4(CLK) and PTG5(MOSI) and GND to logic analyzer.
I think you may need to check the hardware connection.
Best Regards,
Robin
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Robin,
I was not able to see MOSI or clock cycles on the oscilloscope but after changing the buffer size
(bytes of data i’m transferring) values, I can see some signals on it.
1) I see different signals on the oscilloscope if I debug with breakpoint on the SPI_WriteData() function as compared to debug without any breakpoints.
2) Another problem is that, I am seeing less clock and MOSI cycles than expected.(debugging without breakpoints)
for small buffer size (2) I see only one low to high on MOSI and one clock (Yellow - clock, blue - MOSI)
for a large buffer size (100) I see 22 clock cycles as shown below
Shouldnt there be much more MOSI and CLK waveforms as I am transferring 100 bytes of data?
In the above case I kept a fixed baudrate of (baudRate_Bps = 5000U)
but if I increase it to baudRate_Bps = 500000U, I dont get any clock and a low to high transition on MOSI
Could you let me know about these points.
Thanks,