MKE02Z: Configuration and termination for unused GPIO pins

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MKE02Z: Configuration and termination for unused GPIO pins

783 次查看
colin_campbell
Contributor II

Hi NXP,

We are implementing an MKE02Z16VFM4 CPU based design and would like to confirm the recommended GPIO configuration and termination for unused GPIO pins (e.g. Set unused GPIO to Output Low; Set unused GPIO to Input Disabled to reduce power consumption) - the Data Sheet and Reference Manual are silent in this area?

Thanks for the guidance - CC

标记 (2)
0 项奖励
回复
2 回复数

662 次查看
colin_campbell
Contributor II

Hi NXP,

Thanks for the prompt reply and the valuable reference to AN4779 - that all makes sense.

CC

0 项奖励
回复

662 次查看
miduo
NXP Employee
NXP Employee

Hello,

In general, we recommend the unused pins as output low. For unused GPIO it is recommended the following:

 

Do not connect unused I/O pins to anything. Make it floating, and then set it as output low in software. Periodically refresh the state of the pin to avoid changes in state by noise. If floating pins are not allowed in a particular application, connect a 10kΩ pulldown resistor for each unused pin. Do not connect any unused I/O pin to power or ground directly.

 

There has a useful application note for you reference:

https://www.nxp.com/docs/en/application-note/AN4779.pdf