MK64F512x chip readout protection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MK64F512x chip readout protection

1,361件の閲覧回数
chhsu0229
Contributor II

How can I remove the readout protection?

InitTarget()
Protection bytes in flash at addr. 0x400 - 0x40F indicate that readout protection is set.
For debugger connection the device needs to be unsecured.
Note: Unsecuring will trigger a mass erase of the internal flash.
Executing default behavior previously saved in the registry.
Device will be unsecured now.
Timeout while unsecuring device. Erase never starts.
TotalIRLen = 4, IRPrint = 0x01
JTAG chain detection found 1 devices:
#0 Id: 0x4BA00477, IRLen: 04, CoreSight JTAG-DP
DPv0 detected
Scanning AP map to find all available APs
AP[2]: Stopped AP scan as end of AP map has been reached
AP[0]: AHB-AP (IDR: 0x24770011)
AP[1]: JTAG-AP (IDR: 0x001C0000)
Iterating through AP map to find AHB-AP to use
AP[0]: Skipped. Invalid implementer code read from CPUIDVal[31:24] = 0x00
AP[1]: Skipped. Not an AHB-AP

****** Error: Could not find core in Coresight setup

0 件の賞賛
5 返答(返信)

1,305件の閲覧回数
chhsu0229
Contributor II

Hi,

I have tried the way that Kinetis Lock Issue analysis and unlock way.pdf. And, It is unable to unlock MK64F512x.

We produced 250pcs productions using MK64F512x, unfortunately, there are 38pcs were locked. We checked the chip solder temperature. it was ~ 285 degrees. 

I tried to unlock the chip, all showed following debug message,

Connecting to target via SWD
InitTarget()
Protection bytes in flash at addr. 0x400 - 0x40F indicate that readout protectio
n is set.
For debugger connection the device needs to be unsecured.
Note: Unsecuring will trigger a mass erase of the internal flash.
Executing default behavior previously saved in the registry.
Device will be unsecured now.
Timeout while halting CPU.

 

 

0 件の賞賛

1,275件の閲覧回数
PabloAvalos
NXP TechSupport
NXP TechSupport

Hi, @chhsu0229 

 

Many thanks for your patience. Due to holidays the replies were delayed.



Regarding your chip solder temperature around 285 degrees, it is out of spec. You can check it right here: Kinetis K64 Package Quality Tab.

Did the chip reach this peak of 285 degrees of temperature in your production? Because might be damaged.

Please let me know.

 

Best Regards and Happy Holidays.

Pablo Avalos.

0 件の賞賛

1,332件の閲覧回数
PabloAvalos
NXP TechSupport
NXP TechSupport

Hi, @chhsu0229 

 

Many thanks for your patience.

 

Hoping you are well, the method to remove the readout protection can be done by using the GUI Flash Tool that our MCUXpresso IDE supports, and another method can be used is by the SEGGER J-Link Commander.

Here you will find the way to do it using any option that you prefer: https://community.nxp.com/t5/Kinetis-Microcontrollers/MK20DX256VLH7-Jlink-Problem-readout-protection...

 

Please let me know if you have more questions.

 

Best Regards,

Pablo Avalos.

0 件の賞賛

1,323件の閲覧回数
chhsu0229
Contributor II

Hi PabloAvalos,

 

It doesn't work.

 

Thanks

0 件の賞賛

1,313件の閲覧回数
PabloAvalos
NXP TechSupport
NXP TechSupport

Hi, @chhsu0229 

 

Hoping you are excellent.

 

I would like to share with you another alternative that may be help you:

https://community.nxp.com/t5/Kinetis-Microcontrollers/Unable-to-unlock-MKL26z64vft4/m-p/749297

 

Also you can check this guide: Kinetis Lock Issue analysis and unlock way.pdf that it is included into the thread of our community that I provided you above.

 

Please let me know if you have more questions.

 

Best Regards.

Pablo Avalos.

0 件の賞賛