MK20DX256VMC7: I2C's C1 Reigster

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MK20DX256VMC7: I2C's C1 Reigster

Jump to solution
377 Views
huishao2
Contributor IV

Hi-

Inside I2C control register1(i2Cx_C1), bit 7 (IICEN) is used to enable/disable the module. Does a clearing followed by setting on this bit reset all registers in the module back to default status?

Thanks!

Hui

0 Kudos
1 Solution
297 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Hui Shao:

The I2C module registers are not affected by disabling or enabling the I2C module, that only happens with a system reset.

Regards!

Jorge Gonzalez

View solution in original post

0 Kudos
1 Reply
298 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Hui Shao:

The I2C module registers are not affected by disabling or enabling the I2C module, that only happens with a system reset.

Regards!

Jorge Gonzalez

0 Kudos