We will start develop our system using the MKE04Z8VFK4.
Currently we started evaluation using the FRDM-KE04Z and FRDM-KEXX Driver Library Package (REV 1.2.1), but we cannot flash download to the FRDM-KE04Z.
We have the following error message after click "Load" icon in spite of complete build without error.
Load "I:\\Freescale\\Sample Code\\kexx_drv_lib\\build\\keil\\ke04\\Flash_demo\\output\\Flash_demo_Flash.axf"
Error: Flash Download failed - Target DLL has been cancelled
Flash Load finished at 16:32:33
Here is screen shot.
We checked and fixed some settings, but we cannot solve this issue.
If we use IAR EWARM, we can download and debugging correctly.
Therefore, we believe MDK settings are correct.
We uploaded our whole project into below file exchange system.
Could you please advise to solve this issue.
Best regards,
Takashima
Hi Takashima,
Please following the process flow to fix the issue.
Hope it helps.
Have a great day,
Ping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear jeremyzhou,
Thank you for your reply.
I already setup the connection interface, port and settings for connection as below.
But I still have the following error.
Please advise to solve this issue as soon as possible.
Best regards,
Takashima
Hi,
Thanks for your reply.
I've done the more tests, it works well on my site.
So I'd highly recommend you to update the OpenSDA interface with the Segger Jlink firmware application, then select the J-Link instead of the PEMicro Debugger, see the Fig 1.
I've also attached the Jlink firmware.
Fig 1
Have a great day,
Ping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------