MDK-ARM could not flash download to FRDM-KE04Z

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MDK-ARM could not flash download to FRDM-KE04Z

2,403 Views
isaotakashima
Contributor IV

We will start develop our system using the MKE04Z8VFK4.

Currently we started evaluation using the FRDM-KE04Z and FRDM-KEXX Driver Library Package (REV 1.2.1), but we cannot flash download to the FRDM-KE04Z.

We have the following error message after click "Load" icon in spite of complete build without error.

   Load "I:\\Freescale\\Sample Code\\kexx_drv_lib\\build\\keil\\ke04\\Flash_demo\\output\\Flash_demo_Flash.axf"

   Error: Flash Download failed  -  Target DLL has been cancelled

   Flash Load finished at 16:32:33

Here is screen shot.

pastedImage_1.png

We checked and fixed some settings, but we cannot solve this issue.

If we use IAR EWARM, we can download and debugging correctly.

Therefore, we believe MDK settings are correct.

We uploaded our whole project into below file exchange system.

   URL: https://www.teldevice.co.jp/tr2/
   Project Name: KE0x Flash Download Failed
   Expire Date: 2016/12/25
   Account ID: TMP00067615A
   Password: IYpaxHKdFk

Could you please advise to solve this issue.

Best regards,

Takashima

Labels (1)
0 Kudos
3 Replies

1,867 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Takashima,

Please following the process flow to fix the issue.

pastedImage_1.png

pastedImage_2.png

Hope it helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,867 Views
isaotakashima
Contributor IV

Dear jeremyzhou,

Thank you for your reply.

I already setup the connection interface, port and settings for connection as below.

pastedImage_1.png

But I still have the following error.

pastedImage_2.png

Please advise to solve this issue as soon as possible.

Best regards,

Takashima

0 Kudos

1,866 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,

Thanks for your reply.

I've done the more tests, it works well on my site.

So I'd highly recommend you to update the OpenSDA interface with the Segger Jlink firmware application, then select the J-Link instead of the PEMicro Debugger, see the Fig 1.

I've also attached the Jlink firmware.

pastedImage_1.png

                                                                                Fig 1


Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos