Lightweight TCP/IP (lwIP) Stack with SDK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Lightweight TCP/IP (lwIP) Stack with SDK

Lightweight TCP/IP (lwIP) Stack with SDK

Recently I was told that there really lack of enough document && demo regarding the lwIP stack with SDK. So I would like to share more detail regarding this topic, and hope it will been helpful and useful.

Introduction

  • Small independent implementations of the TCP/IP protocol suite
  • One of the most widely used TCP/IP stack
  • Under a BSD-style license
  • Support run in both bare metal and RTOS environment
  • Suitable for use in embedded system with tens of free RAM and room for around 40 kilobytes of code ROM

lwIP stack on KSDK

pastedImage_19.png

    - <ksdk_install_dir>/middleware/tcpip/lwip

lwIP stack on KSDK - Code Structure

  • lwIP code structure is shown as below:

pastedImage_41.png

  • src

    This subfolder includes the latest stable lwIP 1.4.1 source code which can be downloaded from this link: download.savannah.gnu.org/releases/lwip/

  • port

    This subfolder includes the adapter code which adapts lwIP stack to SDK.

lwIP stack on KSDK - Source Code

Structure of source code under is shown below:

pastedImage_56.png

lwIP stack on KSDK – Adapter code

  • <ksdk_install_dir>/middleware/tcpip/lwip/port

pastedImage_64.png

  • <ksdk_install_dir>/middleware/tcpip/lwip/port/arch

pastedImage_70.png

  • These Adapter code could be divided into four types:

        Ethernet driver adapter code

        OSA adapter code

        Additional code

        lwIP stack configuration code

Ethernet Driver Adapter Code

  • Provide Ethernet relevant interface including

   − Ethernet hardware initialization

   − Network interface initialization

   − Send packet to Ethernet hardware

   − Receive packet from Ethernet hardware

   − Pass packet to lwIP stack

  • Both polling and interrupt mode are provided for packet receiving

    - In <ksdk_install_dir>/platform/drivers/inc/fsl_enet_driver.h,

         #define ENET_RECEIVE_ALL_INTERRUPT 0 to enable polling mode.

         Or set

         #define ENET_RECEIVE_ALL_INTERRUPT 1 to enable interrupt mode.

  • Ethernet driver adapter code provides ENET_receive API for polling mode
  • Under RTOS environment, a separate task executing ENET_receive for packet receiving is created in Ethernet hardware initialization code for polling mode
  • Under Bare Metal environment the ENET_receive API need to be called endlessly to do packet receiving

OSA Adapter Code

  • Provide OS dependent types and interface for RTOS environment (configured NO_SYS = 0)

   −Semaphore

   −Mutex

   −Mailbox

   −Thread

  • Provide time tick for bare metal environment(NO_SYS = 1)
  • sys_now to get the current time
  • sys_assert to print an assertion messages and abort execution.

Additional Code

  • Provide definition and interface for:

   −Typedefs

   −Compiler hints for packing and platform specific

   −Diagnostic output

lwIP Stack Configuration Code

  • Provides a way to override much of the behavior of lwIP based on opt.h.

    − Module support (Code size)

          Default inclusions:

    ARP (LWIP_ARP)

    UDP (LWIP_UDP) and UDP-Lite (LWIP_UDPLITE)

    TCP (LWIP_TCP) -- this is a big one!

    Statistics (LWIP_STATS)

         …… 

pastedImage_59.png

        Default exclusions:

   DHCP (LWIP_DHCP)

   AUTOIP (LWIP_AUTOIP)

   SNMP (LWIP_SNMP)

   IGMP (LWIP_IGMP)

   PPP (PPP_SUPPORT)

   − Memory management (RAM usage)

             lwIP’s custom heap-based mem_malloc

             C standard library malloc and free

             Memory pools

lwIP Stack Porting Guide

   Possible Situation for Porting

pastedImage_74.png

New Soc with Limited RAM

In current KSDK, the main RAM consumption for lwIP is show below:

pastedImage_80.png

  • If resource on the new platform is not enough, could reduce ram consumption for ram_heap and pbuf_pool.

        In lwip/port/lwipopts.h:

#define MEM_SIZE                (12*1024)    /**the size of ram_heap/

#define PBUF_POOL_SIZE          10      /*the number of buffers in the pbuf pool. */

#define PBUF_POOL_BUFSIZE       1518 /* the size of each pbuf in the pbuf pool. */

  • pbuf_pool also support dynamically allocate from ram_heap.

       In lwip/include/opt.h:

         #define MEMP_MEM_MALLOC     1 /*Use mem_malloc/mem_free to do allocate*/

  • Use libc malloc/free to manage the memory allocation instead of mem_malloc/mem_free, memory definition for ram_heap is not needed.

        #define MEM_LIBC_MALLOC       1 /*Use malloc/free/realloc provided by C-library*/

  New Soc NOT Support PIT timer

  • OSA adapter code should provide Bare metal lwIP stack with a 1ms period timer. Current the code use pit timer to do this and the definition in sys_arch.c is as below:

#define HWTIMER_LL_DEVIF    kPitDevif      // Use hardware timer PIT

#define HWTIMER_LL_SRCCLK   kBusClock     // Source Clock for PIT

#define HWTIMER_LL_ID       3

#define HWTIMER_PERIOD          1000      // 1 ms interval

  • If the new platform does not provide PIT, we could use other hardware timers to implement the 1ms period timer.

Lightweight TCP/IP (lwIP) Stack Porting v

Lightweight TCP/IP (lwIP) Stack Porting Guide

Lightweight TCP/IP (lwIP) Stack Porting Guide

无评分
版本历史
最后更新:
‎09-28-2015 09:23 PM
更新人: