Hello,
I am using the kl05-FRDM board. I am toggling a pin (LED) pin with the LPTMR0. This timer is clocked by the internal 32KH oscillator.
With a prescaler of 2 (divided by 2). It shld give me at least a period of (1/16000 = 62uSecs). This I did by putting '1' in the LPTMR0_CMR register.
Whenever there is a timeout it toggles a pin. But, always its in mscs and not uSecs.
Is there some error in this. I am posting my code below. Kindly help me
#include "derivative.h" /* include peripheral declarations */
int main(void)
{
int count;
uint16_t countTemp = 0;
SIM_SOPT1 = 0x00040000;
SIM_SCGC5 |= (SIM_SCGC5_LPTMR_MASK | SIM_SCGC5_PORTB_MASK);
PORTB_PCR8 |= 0x00000100; // alternative pin mux selection //
GPIOB_PDDR |= 0x00000100; // pin direction //
SIM_SCGC5|=SIM_SCGC5_LPTMR_MASK;
/* Reset LPTMR settings */
SIM_SOPT1 = 0;
SIM_SCGC5 |= (SIM_SCGC5_LPTMR_MASK | SIM_SCGC5_PORTB_MASK);
LPTMR0_CSR=0;
/* Set the compare value to the number of ms to delay */
//LPTMR0_PSR = LPTMR_PSR_PCS(1)|LPTMR_PSR_PBYP_MASK;
LPTMR0_PSR |=LPTMR_PSR_PBYP_MASK;
//LPTMR0_PSR |=
LPTMR0_CMR = 1;
/* Start the timer */
LPTMR0_CSR |= LPTMR_CSR_TEN_MASK;
/* Wait for counter to reach compare value */
while(1){
while (!(LPTMR0_CSR & LPTMR_CSR_TCF_MASK));
/* Disable counter and Clear Timer Compare Flag */
LPTMR0_CSR &= ~LPTMR_CSR_TEN_MASK;
LPTMR0_CSR |= LPTMR_CSR_TCF_MASK;
GPIOB_PTOR |= (1<<8);
LPTMR0_CSR |= LPTMR_CSR_TEN_MASK;
}
}
解決済! 解決策の投稿を見る。
Hi,
Are you enable internal IRC for LPTimer? You should have the code to enable IRCLK before you enable LPTimer to run. Add following code to have a try?
MCG_C1 |= MCG_C1_IRCLKEN_MASK;
Sandy
Hi,
For Freescale MCUs' clock configuration, it is better to review following chapters of RM once you have any issues:
1. chapter 3 for the IP's clock sources
2. chapter 5 for the MCU clock distribution
3. MCG/OSC chapter for the clock source availability
4. chapter SIM, for the clock switch details mentioned in chapter 3
Thanks,
Sandy
Hi,
Are you enable internal IRC for LPTimer? You should have the code to enable IRCLK before you enable LPTimer to run. Add following code to have a try?
MCG_C1 |= MCG_C1_IRCLKEN_MASK;
Sandy
Thank u.
It works :smileyhappy: