Hi guy.
I'm new about the LPSPI driver.
I'm using a freedom board based up on KEA16Z. I find this kind of SPI port rather difficult. I got some example code to understand this driver, but it'doesn't work jet properly.
I post this code hoping someone can explain why it doesn't work.
The problem is that I can see the tx output data on mosi and the signal clock too on SCKpin
But this happen only for for 8 times.
Infact I call the function every 2 second, and I'd like to see the impulse train just forever every 2 second.
But after 8 transmission the clock pin goes high and the sistem is locked, of course.
Here is the init code, below the call.
void LSPI_Init(void)
{
PCC->CLKCFG[PCC_LPSPI0_INDEX] |= PCC_CLKCFG_CGC_MASK; // PCC->CLKCFG[PCC_PORTE_INDEX] |= PCC_CLKCFG_CGC_MASK; PORTE->PCR[0] = PORT_PCR_MUX(2); //
PORTE->PCR[1] = PORT_PCR_MUX(2); //
PORTE->PCR[2] = PORT_PCR_MUX(2); //
LPSPI0->CR = 0x00000000; /* Disable module for configuration */
LPSPI0->IER = 0x00000000; /* Interrupts not used */
LPSPI0->DER = 0x00000000; /* DMA not used */
LPSPI0->CFGR0 = 0x00000000; /* Defaults: */
/* RDM0=0: rec'd data to FIFO as normal */
/* CIRFIFO=0; Circular FIFO is disabled */
/* HRSEL, HRPOL, HREN=0: Host request disabled */
LPSPI0->CFGR1 = 0x00000001; /* Configurations: master mode*/
/* PCSCFG=0: PCS[3:2] are enabled */
/* OUTCFG=0: Output data retains last value when CS negated */
/* PINCFG=0: SIN is input, SOUT is output */
/* MATCFG=0: Match disabled */
/* PCSPOL=0: PCS is active low */
/* NOSTALL=0: Stall if Tx FIFO empty or Rx FIFO full */
/* AUTOPCS=0: does not apply for master mode */
/* SAMPLE=0: input data sampled on SCK edge */
/* MASTER=1: Master mode */
LPSPI0->TCR = 0x53000008; /* Transmit cmd: PCS3, 16 bits, prescale func'l clk by 4, etc*/
/* CPOL=0: SCK inactive state is low */
/* CPHA=1: Change data on SCK lead'g, capture on trail'g edge*/
/* PRESCALE=2: Functional clock divided by 2 */
/* PCS=3: Transfer using PCS3 */
/* LSBF=0: Data is transfered MSB first */
/* BYSW=0: Byte swap disabled */
/* CONT, CONTC=0: Continuous transfer disabled */
/* RXMSK=0: Normal transfer: rx data stored in rx FIFO */
/* TXMSK=0: Normal transfer: data loaded from tx FIFO */
/* WIDTH=0: Single bit transfer */
/* FRAMESZ=15: # bits in frame = 15+1=16 */
LPSPI0->CCR = 0x0409080A; /* Clock dividers based on prescaled func'l clk of 100 nsec */
/* SCKPCS=4: SCK to PCS delay = 4+1 = 5 (500 nsec) */
/* PCSSCK=4: PCS to SCK delay = 9+1 = 10 (1 usec) */
/* DBT=8: Delay between Transfers = 8+2 = 10 (1 usec) */
/* SCKDIV=8: SCK divider =8+2 = 10 (1 usec: 1 MHz baud rate) */
LPSPI0->FCR = 0x00000001; /* RXWATER=0: Rx flags set when Rx FIFO >0 */
/* TXWATER=3: Tx flags set when Tx FIFO <= 3 */
LPSPI0->CR = 0x00000009; /* Enable module for operation */
/* DBGEN=1: module enabled in debug mode */
/* DOZEN=0: module enabled in Doze mode */
/* RST=0: Master logic not reset */
/* MEN=1: Module is enabled */
}
This every two seconds.
void TestSpi(void)
{
while((LPSPI0->SR & LPSPI_SR_TDF_MASK)>>LPSPI_SR_TDF_SHIFT==0);
LPSPI0->TDR = 0x12;
LPSPI0->SR |= LPSPI_SR_TDF_MASK;
}
Thanks in advance.
Attilio
已解决! 转到解答。
Hi Attillo,
I have noticed that you are creating a master with using a polling method and the FRDM-KE16Z, is this correct?
Being that the case, I believe that taking a look at our SDK LPSPI demos will be worthwhile as a reference. For example lpspi_polling_b2b_transfer.
If you have any issues to download an SDK example, you may check this tutorial
MCU Tech Minutes | Importing an SDK Package into MCUXpresso IDE
This week we had an intense workload, and my reply had been delayed, my apologies!
Please let me know If I can help you further,
BR , Diego
Hi Attillo,
I have noticed that you are creating a master with using a polling method and the FRDM-KE16Z, is this correct?
Being that the case, I believe that taking a look at our SDK LPSPI demos will be worthwhile as a reference. For example lpspi_polling_b2b_transfer.
If you have any issues to download an SDK example, you may check this tutorial
MCU Tech Minutes | Importing an SDK Package into MCUXpresso IDE
This week we had an intense workload, and my reply had been delayed, my apologies!
Please let me know If I can help you further,
BR , Diego