Hello,
I have tried to use a touch screen with a microcontroller MK53DN512CMD10, i'm trying to configure the hardware. It's connected as shown on the table.
TOUCH-SCREEN | MICROCONTROLLER PIN NAME |
---|---|
CS | PTC9 |
RST | PTC10 |
D/C | PTC11 |
WR | PTC12 |
RD | PTC13 |
DB0 | PTC0 |
DB1 | PTC1 |
DB2 | PTC2 |
DB3 | PTC3 |
DB4 | PTC4 |
DB5 | PTC5 |
DB6 | PTC6 |
DB7 | PTC7 |
Y+ | ADC1_DM1/ OP1_DM0 |
Y- | PGA1_DP/ ADC1_DP0/ ADC0_DP3 |
X+ | PGA1_DM/ ADC1_DM0/ ADC0_DM3 |
X- | ADC1_SE16/ OP1_OUT/ CMP2_IN2/ ADC0_SE22/ OP0_DP2/ OP1_DP2 |
LED-A | DAC0_OUT/ CMP1_IN3/ ADC0_SE23/ OP0_DP4/ OP1_DP4 |
And i maded this configuration so far:
#define D4DLCD_CS | 9 |
#define D4DLCD_DC | 11 |
#define D4DLCD_WR | 12 | // WRITECLOCK | |
//#define D4DLCD_WR_PORT | PTED | // WRITECLOCK | |
//#define D4DLCD_WR_DDR | PTEDD | // WRITECLOCK |
#define D4DLCD_RD | 13 | // READCLOCK |
//#define D4DLCD_RD_PORT | PTED | // READCLOCK |
//#define D4DLCD_RD_DDR | PTEDD | // READCLOCK |
#define D4DLCD_RESET | 10 |
/*********** Power macros - for modification uncoment and modify ***********/
// Define void macros, because TWR-K60 board doesn't use RESET pin
#define D4DLCD_INIT_RESET | SIM_SCGC5 |= SIM_SCGC5_PORTC_MASK;\ |
CONFIG_PIN_FUNCTION(C,10,1);\ | |
OUTPUT(C,10) |
#define D4DLCD_ASSERT_RESET WRITE_PIN(C,10,0);
#define D4DLCD_DEASSERT_RESET WRITE_PIN(C,10,1);
// Define void macros, because
#define D4DLCD_INIT_CS | SIM_SCGC5 |= SIM_SCGC5_PORTC_MASK;\ |
CONFIG_PIN_FUNCTION(C,9,1);\ | |
OUTPUT(C,9) |
#define D4DLCD_ASSERT_CS WRITE_PIN(C,9,0);
#define D4DLCD_DEASSERT_CS WRITE_PIN(A,9,1);
// Define void macros, because
#define D4DLCD_INIT_DC | SIM_SCGC5 |= SIM_SCGC5_PORTC_MASK;\ |
CONFIG_PIN_FUNCTION(C,11,1);\ | |
OUTPUT(C,11) |
#define D4DLCD_ASSERT_DC WRITE_PIN(C,11,0);
#define D4DLCD_DEASSERT_DC WRITE_PIN(C,11,1);
// Define void macros, because
#define D4DLCD_INIT_RD | SIM_SCGC5 |= SIM_SCGC5_PORTC_MASK;\ |
CONFIG_PIN_FUNCTION(C,13,1);\ | |
OUTPUT(C,13) |
#define D4DLCD_ASSERT_RD WRITE_PIN(C,13,0);
#define D4DLCD_DEASSERT_RD WRITE_PIN(C,13,1);
// Define void macros, because
#define D4DLCD_INIT_WR | SIM_SCGC5 |= SIM_SCGC5_PORTC_MASK;\ |
CONFIG_PIN_FUNCTION(C,12,1);\ | |
OUTPUT(C,12) |
#define D4DLCD_ASSERT_WR WRITE_PIN(C,12,0);
#define D4DLCD_DEASSERT_WR WRITE_PIN(C,12,1);
#define D4DLCD_INIT_DATA | SIM_SCGC5 |= SIM_SCGC5_PORTC_MASK;\ |
CONFIG_PIN_FUNCTION(C,0,1);\ | |
OUTPUT(C,0);\ | |
CONFIG_PIN_FUNCTION(C,1,1);\ | |
OUTPUT(C,1);\ | |
CONFIG_PIN_FUNCTION(C,2,1);\ | |
OUTPUT(C,2);\ | |
CONFIG_PIN_FUNCTION(C,3,1);\ | |
OUTPUT(C,3);\ | |
CONFIG_PIN_FUNCTION(C,4,1);\ | |
OUTPUT(C,4);\ | |
CONFIG_PIN_FUNCTION(C,5,1);\ | |
OUTPUT(C,5);\ | |
CONFIG_PIN_FUNCTION(C,6,1);\ | |
OUTPUT(C,6);\ | |
CONFIG_PIN_FUNCTION(C,7,1);\ | |
OUTPUT(C,7);\ | |
OUTPUT_ALL(C) |
#endif /* __D4DLCDHW_GPIO8080_8B_CFG_H */
I try to run my code and got stuck on the next function at the d4dlcdhw_common.c file:
static void Cpu_Delay100US(unsigned short us100)
{
unsigned int i;
while((us100--)){
for(i=0; i < (MCU_BUS_CYCLES_100US/10); i++)
{// 10 cycles delay
asm("NOP");
asm("NOP");
asm("NOP");
}
}
}
¿Is my configuration correct?
¿how do i configure the adc for the touch-screen?
¿how do i use the DAC output for the backlight ?
I will apreciate a lot your help !!!!!
Regards
解決済! 解決策の投稿を見る。
Hello Alberto,
I saw that there is another thread with the same question D4D library troubles using a touch-screen LCD / MK53DN512CMD10 microcontroller, I will be answering there, is that OK?
Best regards,
Earl.
Hello Alberto,
Which touchscreen are you using? Are you migrating from another project?
Best regards,
Earl.
Hi Earl,
Thanks for your answer. I'm using a touchscreen model NHD-1.8-128160EF-CTXI-T and yes i'm migrating form another project.
I left the link of the datasheet below.
Regards
Alberto
http://www.newhavendisplay.com/specs/NHD-1.8-128160EF-CTXI.pdf
Hello Alberto,
I saw that there is another thread with the same question D4D library troubles using a touch-screen LCD / MK53DN512CMD10 microcontroller, I will be answering there, is that OK?
Best regards,
Earl.
OK,thank you.
Regards