Kinetis K82P121M150SF5RM based TWR-POS-K81, QuadSPI skips a bit while reading from N25Q256A

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis K82P121M150SF5RM based TWR-POS-K81, QuadSPI skips a bit while reading from N25Q256A

1,133件の閲覧回数
bvsrkrishnarao
Contributor II

Hi

I am working on Kinetis K82P121M150SF5RM based TWR-POS-K81 board with N25Q256A, while reading the status/ReadID/Configuration register in extended SPI mode, the K82 QuadSPI module seems to skip a bit

for example

while reading ReadID from N25Q256A the expected bytes are 20 BA 19 10 ...

but the actual bytes I am receiving are 10 5D 08 (it is off by a bit)

Is there anything I am missing?

The TWR-POS-K81 seems to be very flaky. sometimes the data seems to be receiving from the N25Q256A allright and the very next iteration, I see all junk coming for the same command like ReadID or read Status Register.

Any thoughts or insights on this will be great help

thanks

Krishna

0 件の賞賛
返信
4 返答(返信)

651件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Krishna,

How did you initialize the qspi module? Would you please share some code or register dump for it? Thanks for your patience!


Have a great day,
Kan

NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

651件の閲覧回数
bvsrkrishnarao
Contributor II

Hi Kan

Download the below development software from these links if you don't

allready have them.

1. Kinetis Build Environment (KDS 3.0)

(Kinetis Design Studio installer for Microsoft Windows 3.0.0)

Use the link below to dwnload Kinetis Design Studio

http://www.nxp.com/products/software-and-tools/run-time-software/kinetis-software-and-tools/ides-for...

2.Download the Kinetis SDK 1.3.0

(Kinetis SDK 1.3.0 Mainline - Windows)

http://www.nxp.com/products/software-and-tools/run-time-software/kinetis-software-and-tools/developm...

3.Download the "Kinetis SDK 1.3.0 Standalone for the FRDM-K82F - Windows"

https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&element=6912747

https://freescaleesd.flexnetoperations.com/337170/437/9280437/Kinetis%20SDK%201.3.0%20Standalone%20f...

After installing 1 & 2 in directory C:\Freescale

Unzip #3 to KSDK_1.3.1

After the above steps

Open KDS (Kinetis Design Studio)

1. Load Project "ksdk_platform_lib_K82F25615"

Goto "File"->"Ïmport" dialog

Under "General" select "Existing Projects Into Workspace" Press "Next"

"Select Root Directory" Browse and select

"C:\Freescale\KSDK_1.3.1\lib\ksdk_platform_lib\kds\K82F25615"

2. Load Project "qspi_example_frdmk82f"

Goto "File"->"Ïmport" dialog

Under "General" select "Existing Projects Into Workspace" Press "Next"

"Select Root Directory" Browse and select

"C:\Freescale\KSDK_1.3.1\examples\frdmk82f\driver_examples\qspi\kds"

Using "Project Explorer" (Top Left Corner)

Right click on the "ksdk_platform_lib_K82F25615" and select "Build Project"

next step Right click on the "qspi_example_frdmk82f" and select "Build

Project"

Verify if you have a "qspi_example_frdmk82f.elf" under directory

"C:\Freescale\KSDK_1.3.1\examples\frdmk82f\driver_examples\qspi\kds\debug"

The Qspi driver examples are in the

"C:\Freescale\KSDK_1.3.1\examples\frdmk82f\driver_examples\qspi\main.c"

If you have a debugger (ours is a j-Link debugger) and a Freescale board,

we have TWR-POS-K81, one can download and debug/go through the code

let me know if you have any issues (the above example code should work with

some limitations)

regards

Krishna

On Tue, Feb 2, 2016 at 8:43 AM, Kan_Li <admin@community.freescale.com>

0 件の賞賛
返信

651件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Krishna,

I have checked with the KSDK team, the board TWR-POS-K81 has different external flash from what on FRDM-K82F, so To run the qspi example, all flash command is different and shall be changed. Also the UART port and other board settings need to be changed. but we also provide a special KSDK software package for it, which is just available for customers under NDA, please contact your local DFAE for assistance on NDA issue. Please kindly refer to Distributor Network|NXP for more details.

Hope that helps,


Have a great day,
Kan

NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

651件の閲覧回数
bvsrkrishnarao
Contributor II

Hi Kan

Thanks a lot for the response

we were intimated by our client about the special package for TWR-POS-K81

board, and our company is currently engaged with NXP/Freescale in getting

those formalities done.

Thanks again

regards

Krishna

On Thu, Feb 18, 2016 at 7:39 AM, Kan_Li <admin@community.freescale.com>

0 件の賞賛
返信