I have KL26Z Eval board. I can't upgrade it and it doesn't work if it is nowmally connected. It is only work on the bootloader mode. What can I do?
Hello ,
When you insert the USB to J10 , do not press any button .
You also can refer to the quick start guide.
If still can not work ,please take a photo or video show me how do you
operate and the result .
Hope it helps
Have a great day,
Alice
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Ok, don't warrior ,which IDE do you used ? you can create one simple project to test.
And you can check the "Device Manager" of computer to check which debug way ,
for example , on my side , it is PE debug:
Have a great day,
Alice
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Oh, i have told you , please refer to the Quick start i have send you update the bootlader,,
Have a great day,
Alice
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I did it. It works! The problem was Windows 8.1 . If your bootloader 1.10 or early, you have to do all
on Windows 7 or Xp. I tried it on windows 7 and it worked. Thank you very much... :smileyhappy: