I am trying to route the output of the PLL to clock the UART0. In the ref manual, chapter 5 page 117, clocking options for UART0 are shown as below:
But I could not find PLLFLLSEL bits in the SIM_SOPT2. The description of SIM_SOPT2 is shown as below (Section 12.2.3 page 186):
Anyone know are these bits implemented for KL15 chips?
thanks!
解決済! 解決策の投稿を見る。
Hi, Safwat
This is a document issue. The bit 16 in register SIM_SOPT2 is PLLFLLSEL.
Hope my reply can help you.
Best Regards
Paul
Thanks Paul. Good to know its there :smileyhappy:
Hi, Safwat
This is a document issue. The bit 16 in register SIM_SOPT2 is PLLFLLSEL.
Hope my reply can help you.
Best Regards
Paul
The SIM_SOPT2_PLLFLLSEL bit is also missing in Processor Expert generated file (IO_Map.h):
/* SOPT2 Bit Fields */
#define SIM_SOPT2_RTCCLKOUTSEL_MASK 0x10u
#define SIM_SOPT2_RTCCLKOUTSEL_SHIFT 4
#define SIM_SOPT2_CLKOUTSEL_MASK 0xE0u
#define SIM_SOPT2_CLKOUTSEL_SHIFT 5
#define SIM_SOPT2_CLKOUTSEL(x) (((uint32_t)(((uint32_t)(x))<<SIM_SOPT2_CLKOUTSEL_SHIFT))&SIM_SOPT2_CLKOUTSEL_MASK)
#define SIM_SOPT2_TPMSRC_MASK 0x3000000u
#define SIM_SOPT2_TPMSRC_SHIFT 24
#define SIM_SOPT2_TPMSRC(x) (((uint32_t)(((uint32_t)(x))<<SIM_SOPT2_TPMSRC_SHIFT))&SIM_SOPT2_TPMSRC_MASK)
#define SIM_SOPT2_UART0SRC_MASK 0xC000000u
#define SIM_SOPT2_UART0SRC_SHIFT 26
#define SIM_SOPT2_UART0SRC(x) (((uint32_t)(((uint32_t)(x))<<SIM_SOPT2_UART0SRC_SHIFT))&SIM_SOPT2_UART0SRC_MASK)
/* SOPT4 Bit Fields */