KL05 ,PTA13 ,can't enable pull down

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KL05 ,PTA13 ,can't enable pull down

458 Views
diegocolombo
Contributor IV

Hi

reading the KL05 reference manual i can't find any reason why  PTA13 could not have the pull down enabled.

Moving it by hand in debug mode it can't be set to 0.

Is there any errata about it or is it my fault??

Thanks

Labels (1)
0 Kudos
1 Reply

366 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Diego:

This is not an errata. In your KL05 you can only enable Pull Up, but cannot select Pull Down. You can confirm this in the Chip Configuration -> Human Machine Interfaces chapter. See below:

pastedImage_5.png

I hope this clarifies.

Regards!,

Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos