KL series LIN slave simply usage sharing

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

KL series LIN slave simply usage sharing

KL series LIN slave simply usage sharing

1 Abstract

     LIN (Local Interconnect Network) is a concept for low cost automotive networks, which complements the existing portfolio of automotive multiplex networks. LIN is based on the UART/SCT protocol. It can be used in the area of automotive, home appliance, office equipment, etc. The UART module in NXP kinetis L series contains the LIN slave function, it can be used as the LIN slave device in the LIN bus. Because there is few LIN slave KL sample code for the customer’s reference in our website, now this document mainly take KL43 as an example, explain how to use the FRDM-KL43 board as the LIN slave node to communicate with the LIN master device. LIN master use the specific LIN module: PCAN-USB Pro FD. Master send the publisher ID and subscriber ID, slave give the according LIN data response. This document will share the according code, hardware connection and the test result.

2 LIN bus basic knowledge review

        For the convenient to understand the LIN bus, this chapter simply describe the basic knowledge for LIN bus. Mainly about the LIN topology and the LIN frame.

2.1 LIN bus topology structure

      LIN bus just use the simple low cost single-wire, it uses single master to communicate with multiple slaves. The bus voltage is 12V, the speed can up to 20 kbit/s. LIN network can connect 16 nodes, but in the practical usage, normally use below 12 nodes.

186555_186555.pngpastedImage_2.png

Figure 2-1. LIN bus topology

2.2 LIN bus frame structure     

    LIN Frame consists of a header (provided by the master task) and a response (provided by a slave task).

    Master send publisher frame: Master send header+ data +checksum; slave just receive.

    Master send subscriber frame: Master send header; slave receive send data +checksum.

    The following figure is the structure of a LIN frame:

186554_186554.pngpastedImage_3.png

Figure 2-2. LIN frame structure

     LIN frame is constructed of one Break field, sync byte field (0X55), PID, data and checksum.

2.2.1 Break filed and break delimiter

Break filed is consist of break and break delimiter. Break should at least 13 nominal bit times of dominant value (low voltage). The break delimiter shall be at least one nominal bit time long (high voltage).

186535_186535.pngpastedImage_6.png

Figure 2-3. break field

2.2.2 Sync byte field

Sync is a byte field with the data value 0X55. The byte field is the standard UART protocol.

186556_186556.pngpastedImage_10.png

Figure 2-4. The sync byte field

2.2.3 Protected identifier field

A protected identifier field consists of two sub-fields: the frame identifier and the parity. Bits 0 to 5 are the frame identifier and bits 6 and 7 are the parity.    

ID value range: 0x00-0x3f, 64 IDs in total. It determine the frame categories and direction.

186557_186557.pngpastedImage_12.png

Figure 2-5. The sync byte field

P0 = ID0 xor ID1 xor ID2 xor ID4

P1 = -(ID1 xor ID3 xor ID4 xor ID5)

-is NOT

 ID can be split in three categories:

 

Frame categories

Frame ID

Signal carrying frame

Unconditional frame

0x00-0x3B

Event triggered frame

Sporadic frame

Diagnostic frame

Master request frame

0x3c

Slave response frame

0x3d

Reserved frame

 

0x3e,0x3f

 

 

2.2.4 DATA

      A frame carries between one and eight bytes of data. The number of data contained in a frame with a specific frame identifier shall be agreed by the publisher and all subscribers.

     For data entities longer than one byte, the entity LSB is contained in the byte sent first and the entity MSB in the byte sent last (little-endian). The data fields are labeled data 1, data 2,... up to maximum data 8.

2.2.5 checksum 

The checksum contains the inverted eight bits sum with carry over all data bytes or all data bytes and the protected identifier.       

Classic checksum: Checksum calculation over the data bytes.

Enhanced checksum: Checksum calculation over the data bytes and the protected identifier byte.

 Method: eight bits sum with carry is equivalent to sum all values and subtract 255 every time the sum is greater or equal to 256, at last, the sum data do bitwise invert.  In the receive side, do the same sum, but at last, don’t do invert, then add the received checksum data, if the result is 0XFF, it is correct, otherwise, it is wrong.

3 KL43 LIN slave example

   This chapter use KL43 as the LIN slave, and communicate with the specific LIN master device, realize the LIN data sending and receiving.

3.1 Hardware prepare

Hardware: FRDM-KL43TRK-KEA8PCAN-USB Pro FD

      LIN bus voltage is 12V, but the FRDM-KL43 don’t have the LIN transceiver, so we need the external LIN transceiver connect the KL43 uart, to realize the LIN voltage switch. Here we use the TRK-KEA8 on board LIN transceiver MC33662LEF for the KL43. The MC33662LEF circuit is like this:

   186558_186558.pngpastedImage_14.png

Figure 3-1. LIN transceiver schematic

3.1.1 FRDM-KL43 and TRK-KEA8 connections

     FRDM-KL43 need to connect the UART port to the LIN transceiver. The connection shows in this table:

No.

FRDM-KL43

TRK-KEA8

note

1

J1-2

J10-5

UART0_RX

2

J1-4

J10-6

UART0_TX

3

J3-14

J14-1

GND

3.1.2 TRK-KEA8 and LIN master connections

        LIN bus is using the signal wire.  TRK-KEA8 J14_4 is the LIN wire, it should connect with the LIN wire in PCAN-USB Pro FD. GND also need to connect together.

       TRK-KEA8 P1 need a 12V DC supplier. Master also need 12V DC supplier.

3.1.3 Object connection picture

 186562_186562.pngpastedImage_19.png

Figure 3-2. Object connections

3.2 Software flow chart and code

     Now describe how to realize the LIN master and the LIN slave data transfer. LIN master send a publisher frame, the slave will receive the according data. LIN master send a subscriber frame, the slave will send the data to the master. The code is based on the KSDK2.2_FRDM-KL43 lpuart, add the LIN operation code.

 3.2.1 Software flow chart

 186559_186559.pngpastedImage_20.png

     

Figure 3-3. Software flow chart

 

3.2.2 software code

    Code is based on KSDK2.2_FRDM-KL43 lpuart project, add the LIN operation code, the added code is list as follows:

void LPUART0_IRQHandler(void)

{

     if(LPUART0->STAT & LPUART_STAT_LBKDIF_MASK)

     {

       LPUART0->STAT |= LPUART_STAT_LBKDIF_MASK;// clear the bit

       Lin_BKflag = 1;

       cnt = 0;

       state = RECV_SYN;

       DisableLinBreak;    

     }

    if(LPUART0->STAT & LPUART_STAT_RDRF_MASK)

     {

                 rxbuff[cnt] = (uint8_t)((LPUART0->DATA) & 0xff);        

         switch(state)

         {

            case RECV_SYN:

                          if(0x55 == rxbuff[cnt])

                          {

                              state = RECV_PID;

                          }

                          else

                          {

                              state = IDLE;

                              DisableLinBreak;

                          }

                          break;

            case RECV_PID:

                          if(0xAD == rxbuff[cnt])

                          {

                              state = RECV_DATA;

                          }

                          else if(0XEC == rxbuff[cnt])

                          {

                              state = SEND_DATA;

                          }

                          else

                          {

                              state = IDLE;

                              DisableLinBreak;

                          }

                          break;

            case RECV_DATA:

                          recdatacnt++;

                          if(recdatacnt >= 4) // 3 Bytes data + 1 Bytes checksum

                          {

                              recdatacnt=0;

                              state = RECV_SYN;

                              EnableLinBreak;

                          }

                          break;

         default:break;

                         

         }        

         cnt++;

     }    

}

void uart_LIN_break(void)

{

    LPUART0->CTRL &= ~(LPUART_CTRL_TE_MASK | LPUART_CTRL_RE_MASK);   //Disable UART0 first

    LPUART0->STAT |= LPUART_STAT_BRK13_MASK; //13 bit times

LPUART0->STAT |= LPUART_STAT_LBKDE_MASK;//LIN break detection enable

LPUART0->BAUD |= LPUART_BAUD_LBKDIE_MASK;

   

    LPUART0->CTRL |= (LPUART_CTRL_TE_MASK | LPUART_CTRL_RE_MASK);

    LPUART0->CTRL |= LPUART_CTRL_RIE_MASK;

    EnableIRQ(LPUART0_IRQn);   

}

int main(void)

{

    uint8_t ch;

    lpuart_config_t config;

    BOARD_InitPins();

    BOARD_BootClockRUN();

    CLOCK_SetLpuart0Clock(0x1U);

    LPUART_GetDefaultConfig(&config);

    config.baudRate_Bps = BOARD_DEBUG_UART_BAUDRATE;

    config.enableTx = true;

    config.enableRx = true;

    LPUART_Init(DEMO_LPUART, &config, DEMO_LPUART_CLK_FREQ);

    uart_LIN_break();

    while (1)

    {

       if(state == SEND_DATA)

       {

          while((LPUART0->STAT & LPUART_STAT_TDRE_MASK) == 0); // hex mode

                  LPUART0->DATA = 0X01;

          while((LPUART0->STAT & LPUART_STAT_TDRE_MASK) == 0); // hex mode

                  LPUART0->DATA = 0X02;

          while((LPUART0->STAT & LPUART_STAT_TDRE_MASK) == 0); // hex mode

                  LPUART0->DATA = 0X10;//Checksum   0X10 correct, 0xaa is wrong

          recdatacnt=0;

          state = RECV_SYN;

          EnableLinBreak;

       }

    }

}

 

 

4 KL43 LIN slave test result

  Master defines two frames:

Unconditional ID

Protected ID

Direction

Data

checksum

0X2C

0XEC

subscriber

0x01,0x02

0x10

0X2D

0XAD

Publisher

0x01,0x02,0x03

0x4c

   Now, master send 0X2C and 0X2D data, give the test result and the according waveform.

4.1 LIN master configuration

Uart baud rate is: 9600bps

186561_186561.pngpastedImage_22.png

4.2  Send ID 0X2C and 0X2D frame

 

186569_186569.jpgpastedImage_1.jpg

    From the PC software of LIN master, we can find 0X2D ID can send the data successfully, and 0X2C ID can receive the correct data (0x01, 0x02) and checksum (0x10) from the KL43 LIN slave side.

4.2.1 0X2D ID frame oscilloscope waveform and debug result

186564_186564.pngpastedImage_24.png

 

186570_186570.jpgpastedImage_2.jpg

   From the debug result, we can find the buff can receive the correct ID, data and checksum from the LIN master.  

 4.2.2 0X2C ID frame oscilloscope waveform

186566_186566.pngpastedImage_26.png

4.2.3 0X2C ID SLAVE send back the wrong checksum

 

186571_186571.jpgpastedImage_3.jpg

  From the PC software, we can find if the KL43 code modify the checksum to the wrong data 0XAA, then the PC software will display the checksum error.

This is the according oscilloscope waveform for the wrong checksum data.

186568_186568.pngpastedImage_28.png

From all the above test result. We can find, KL43 as the LIN slave, it can receive the correct data from the LIN master, and when LIN master send the subscriber ID, kl43 also can send back the correct LIN data to the master. More detail, please check the attached code project.

BTW, LIN spec can be downloaded from this link:

http://www.cs-group.de/wp-content/uploads/2016/11/LIN_Specification_Package_2.2A.pdf

 

Attached is the code and the pdf version of this document:

 

 

             

标签 (1)
附件
无评分
版本历史
最后更新:
‎06-12-2017 01:41 AM
更新人: