hI,everyone,I'm design an easy uart bootloader on KL14,the test bootloader has only jump code ,which is bellow:
// relocate vector table
SCB_VTOR = RELOCATED_VECTORS;//0x10000;
// Jump to user application
JumpToUserApplication((RELOCATED_VECTORS),(RELOCATED_VECTORS+4));//*(unsigned long*) //*((unsigned long*)
JumpToUserApplication
msr msp, r0
msr psp, r0
mov pc, r1
END
but it almost never works. I said almost because once it works,it succeed in jumps to where my application locates and it works! but one day later,after some flash changing,
I can never make it work again.
SO now,I wonder if it's because my scf file which decides my code's placement under KEIL.
I want to locate it in 0x10000,so I move the userapp's bin file entirely to this address.
Is it ok?or how should I modify it?
Really appreciate your help,I've worked for a whole week!
已解决! 转到解答。
Hi,Kan, sorry for replying late.Thanks for your help.
Now I've known the answer.the user code should be loaded in the moved address.for example 0x1000;
then your sct file should be like this:
LR_IROM1 0x00001000 0x00020000 { ; load region size_region
ER_IROM1 0x00001000 0x00020000 { ; load address = execution address
*.o (RESET, +First)
*(InRoot$$Sections)
.ANY (+RO)
}
RW_IRAM1 0x1FFFF000 0x00001000 { ; RW data
.ANY (+RW +ZI)
}
RW_IRAM2 0x20000000 0x00003000 { ; RW data
.ANY (+RW +ZI)
*(runinram)
}
}
attach my scf file bellow:(128K flash,16K RAM):
; *************************************************************
; *** Scatter-Loading Description File generated by uVision ***
; *************************************************************
LR_IROM1 0x00000000 0x00020000 { ; load region size_region
ER_IROM1 0x00000000 0x00020000 { ; load address = execution address
*.o (RESET, +First)
*(InRoot$$Sections)
.ANY (+RO)
}
RW_IRAM1 0x1FFFF000 0x00001000 { ; RW data
.ANY (+RW +ZI)
}
RW_IRAM2 0x20000000 0x00003000 { ; RW data
.ANY (+RW +ZI)
*(runinram)
}
}
Hi Fu Grace,
Please kindly refer to page 30 of http://cache.freescale.com/files/microcontrollers/doc/app_note/AN2295.pdf for more details on memory allocation. You may find bootloader demos for KL part in "an2295sw\src\Kinetis\KEIL_uV4" which is from an2295sw.zip(http://cache.freescale.com/files/microcontrollers/doc/app_note/AN2295SW.zip) .
Hope that helps,
Have a great day,
Kan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,Kan, sorry for replying late.Thanks for your help.
Now I've known the answer.the user code should be loaded in the moved address.for example 0x1000;
then your sct file should be like this:
LR_IROM1 0x00001000 0x00020000 { ; load region size_region
ER_IROM1 0x00001000 0x00020000 { ; load address = execution address
*.o (RESET, +First)
*(InRoot$$Sections)
.ANY (+RO)
}
RW_IRAM1 0x1FFFF000 0x00001000 { ; RW data
.ANY (+RW +ZI)
}
RW_IRAM2 0x20000000 0x00003000 { ; RW data
.ANY (+RW +ZI)
*(runinram)
}
}