KE04(或 KL17) 烧录后复位问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KE04(或 KL17) 烧录后复位问题

810 Views
jimmyli
Contributor IV

 问题1:将代码通过J-Link烧录到KE04目标板(MCU一直外部供电,且代码中设置上电后MCU处于stop模式),完成后拔掉SWD接插口,此时MCU耗电3mA(3.3V供电);按外部Reset引脚,重新复位,电流也是3mA;给MCU重新掉电和上电后,此时整体电流变为0.023mA。

        注:MCU引脚均没有外接其他电路。

问题2:将代码通过J-Link,采用安全模式下载代码,完成后按MCU Reset键无效;只有重新掉电、上电后,MCU才能正常工作和复位。

        注:非安全模式下载是可以的,如问题1现象。

谢谢!

Labels (2)
0 Kudos
4 Replies

549 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

你好!

如果你那里有FRDM-KE04板子,相关代码下载到FRDM板子里,会不会复现上述情况?

通过你的描述,问题1是KE04无法正常退出复位模式,进入STOP模式。

请将你的代码在FRDM-KE04板子上试一下,看下具体现象。


Have a great day,
Mike

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

549 Views
jimmyli
Contributor IV

Hi Mike,

     我手里没有FRDM-KE04,只有客户的目标板,目前还没有找到原因。

     现在想了解具体有哪些模块无法在代码烧录并带电复位后,哪些模块无法被正常关闭。(只有POR才能做到)

     目前已测试上电后,代码会关掉DEBUG模块,但效果一样。

     谢谢!

0 Kudos

549 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Jimmy,

请查看代码,是否SWD相应的管脚设置为其他功能,如果这样的话,芯片上电后调试口就无法使用。

另外,通过上拉电阻将PTB4(/NMI)管脚上拉至VDD,看看情况是否有改善。


Have a great day,
Mike

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

549 Views
jimmyli
Contributor IV

Hi Mike,

     谢谢你的提醒,我这边再试一下。

0 Kudos