KE02: Internal Clock Source: IRC in FEI Mode: Impact of Maximum Frequency

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

KE02: Internal Clock Source: IRC in FEI Mode: Impact of Maximum Frequency

850 次查看
colin_campbell
Contributor II

Hi NXP,

Our MKE02Z64VFM4 clock configuration uses the Internal Reference Clock (IRC) in FEI Mode, with the the IRC to 39.0625 kHz and the FLL Multiplier set to 1024, to obtain a nominal maximum clock frequency of 40 MHz. We have not undertaken additional trimming of the Internal Clock Source, and are therefore reliant on the accuracy of the production trimming (+/- 0.5%).

In our application, we have seen repeatable resets of the CPU when the case temperature of the CPU is >= 100C. We have inspected the CPU SIM_SRSI Reset Source Register and confirmed that the source of the reset is the internal Watchdog.

Our reading of section 20.4.5 of the KE02 Family Reference Manual suggests that this behaviour is probably due to our core clock frequency exceeding the maximum allowable value of 40 MHz (noting the IRC Trim accuracy of +/- 0.5%), which is then followed by a Firmware lockup state with a subsequent assertion of the Watchdog and CPU reset – could you please provide a response to the following questions:

  1. What is the expected system behaviour when the maximum core clock frequency is exceeded?
  2. Are there any known limitations/errata that have been published for operation of the KE02 devices at high temperatures and (Tcase >= 100C) and at high clock frequencies (e.g. 40 MHz)?

Thank you for the assistance - CC

标签 (1)
0 项奖励
回复
2 回复数

741 次查看
Alexis_A
NXP TechSupport
NXP TechSupport

Hi Colin,

Check my answers bellow,

  1. What is the expected system behaviour when the maximum core clock frequency is exceeded?

As you mention this is outside the spec and isn't caracterized but as a test could you try using a lower operation frequency to check if this error also appears?

  1. Are there any known limitations/errata that have been published for operation of the KE02 devices at high temperatures and (Tcase >= 100C) and at high clock frequencies (e.g. 40 MHz)?

Until now there isn't any erratas regarding this issue. You could check this document to know which erratas where found.

Best Regards,

Alexis Andalon

741 次查看
colin_campbell
Contributor II

Hi Alexis,

Thank you for the prompt feedback - that all makes sense.\

The Errata does not currently include any relevant details for our test condition, and we are proceeding with a lower core clock frequency test.

Many thanks for the assistance - CC

0 项奖励
回复