K66 USB Host, USBHS_USBINTR_NAKE doesn't seem to actually exist?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K66 USB Host, USBHS_USBINTR_NAKE doesn't seem to actually exist?

838 Views
frankzhao_sony
Contributor I

Processor is a MK66FX1M0, reference manual is K66P144M180SF5RMV2.pdf

(actually using a Teensy 3.6 with USBHost_t36 library)

USBHS is running in host mode, at high-speed

Page 1606 section 54.3.17 USB Interrupt Enable Register (USBHS_USBINTR)

The bit is 16, NAKE, NAK Interrupt Enable

 

#define USBHS_USBINTR		(*(volatile uint32_t *)0x400A1148) // USB Interrupt Enable Register
#define USBHS_USBINTR_TIE1		((uint32_t)0x02000000)
#define USBHS_USBINTR_TIE0		((uint32_t)0x01000000)
#define USBHS_USBINTR_UPIE		((uint32_t)0x00080000)
#define USBHS_USBINTR_UAIE		((uint32_t)0x00040000)
#define USBHS_USBINTR_NAKE		((uint32_t)0x00010000)

 

 

I have a rather odd project that requires me to handle the case when a bulk packet is sent from host-to-device (OUT) but receives a NAK and handle that case immediately instead of waiting for more NAKs. This ISR is not firing even though I have set both USBHS_USBINTR_NAKE and the corresponding bits in the USBHS_ENDPTNAKEN registers

Debugging further to find a root cause, it seems like: the place inside USBHS_USBINTR where USBHS_USBINTR_NAKE should be simply does not exist (like a reserved bit). Writing into it and reading it back out, bit position 16 is always zero.

 

Example code

 

#include "USBHost_t36.h"

USBHost myusb;

USBHIDParser hid1(myusb);

USBDriver *drivers[] = { &hid1, };
#define CNT_DEVICES (sizeof(drivers)/sizeof(drivers[0]))
const char* driver_names [CNT_DEVICES] = { "hid1", };
      bool  driver_active[CNT_DEVICES] = { false, };

void setup()
{
  while (!Serial && (millis() < 5000)) ; // wait for Arduino Serial Monitor
  Serial.println("\n\nUSB Host Testing USBHS_USBINTR_NAKE");
  myusb.begin();
}

void loop()
{
  myusb.Task();
  USBHS_USBINTR |= (1 << 16); // explicitly use the number 16 instead of USBHS_USBINTR_NAKE
  if ((USBHS_USBINTR & (1 << 16)) == 0)
  {
    Serial.printf("Error: NAKE not written, 0x%08X\n", USBHS_USBINTR);
    delay(500);
  }
}

 

 

The NAKE bit fails to be written, the register reads back as 0x030C0016, what is expected is 0x030D0016

Another try

 

#include "USBHost_t36.h"

USBHost myusb;

USBHIDParser hid1(myusb);

USBDriver *drivers[] = { &hid1, };
#define CNT_DEVICES (sizeof(drivers)/sizeof(drivers[0]))
const char* driver_names [CNT_DEVICES] = { "hid1", };
      bool  driver_active[CNT_DEVICES] = { false, };

void setup()
{
  while (!Serial && (millis() < 5000)) ; // wait for Arduino Serial Monitor
  Serial.println("\n\nUSB Host Testing USBHS_USBINTR_NAKE");
  myusb.begin();
}

void loop()
{
  myusb.Task();

  USBHS_USBINTR = 0xFFFFFFFF;
  Serial.printf("USBHS_USBINTR: 0x%08X\n", USBHS_USBINTR);
  delay(500);
}

 

 

The register reads back as 0x030C00BF, but I expected 0x030D00BF if bit position 16 was writable

What is going on? Where is USBHS_USBINTR_NAKE? How do I generate a ISR when I get a NAK?

(NOTE: there is no code that clears USBHS_USBINTR without me knowing about it)

(NOTE: I have tried writing to USBHS_ENDPTNAKEN before writing to USBHS_USBINTR, it does NOT help)

(NOTE: I am using a USB HS analyzer, TotalPhase Beagle USB 480, I can see every single ACK, NAK, SOF, ping, etc)

(NOTE: I checked the errata about this)

Thanks

Frank

Labels (2)
0 Kudos
1 Reply

819 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @frankzhao_sony ,

The USB_USBINTR[NAKE] bit is for device mode only. In host mode, this bit can't write. You can download K66 SDK and compare in host and device demo in the SDK.

 

Regards,

Jing

0 Kudos